Part Number: TPS563219A Hello,
Could you help to elaborate what is "Make a Kelvin connection to the GND pin for the feedback path"?
This is one of layout rules which from TPS563219A datasheet.
It will be better if you can introduce it with…
Part Number: TPS563219A Dear Team
We have a question about how to do TPS563219A OVP test and measurement?
Here's the test method we did.
Method#1: Inject a 1.1V voltage source at VFB pin.
Test result:
The SW indeed terminated after injecting by…
Part Number: TPS563219A Hello,
My customer would like to use TPS563219ADDFR.
They are asking if this device have overvoltage/undervoltage protection function for Vin and Vout.
Could you kindly tell me the answer, please?
Best regards,
K.Hirano
Part Number: TPS563219A Hi
Please let me ask you about Cout value of TPS563219A.
My customer use about 100uF as Cout.
But the recommending Cout value is 20~68uF in datasheet.
May I use this device with that's Cout?
The customer's condition is Vin…
Part Number: TPS563219A Hello,
I have a question for TPS563219ADDFR package information.
From the datasheet(SLVSDP9), there is a package outline page, P28.
The below is from the page.
In this picture, please see blue and red marked values.
There…
Part Number: TPS563219A WEBENCH gave me a design which uses the TPS563219 IC as the controller. However, the page says that chip is not recommended for new designs, and suggests using the TPS563219A instead. I checked the datasheets and it seems like the…
Part Number: TPS563219A Other Parts Discussed in Thread: TPS568215 Hi
My customer has question.
■TPS563219A
Is it OK if connecting the EN terminal with 3.3 V logic only by connecting with 10 kΩ?
■TPS568215
Is it OK to control the EN pin of TPS568215A…
Part Number: TPS563219A Hi,
Can you please help me in identifying the difference between TPS563219A, TPS563219. As from datasheet i can see that operating temperature of both is -40 to 85 deg c.
Thanks
Phani