Part Number: TPS563231 Tool/software: Dear Specialists,
My customer is considering TPS563231 and has a question about Rboot.
I have considered the value of Rboot.
Please confirm the listed below.
I have focused on the rise time, I think the result may…
Part Number: TPS563231 Dear Specialists,
My customer is considering TPS563231 and has a question.
I would be grateful if you could advise.
---
・We are planning to use a 3.6uH inductance for 3.8V output.
If 3.6uH is not appropriate, please let me know…
Part Number: TPS563231 HI experts,
On DS for TPS563231DRLR, it seems that there are no TAPE AND REEL INFO as below. Could you share us the same one about TPS563231DRLR?
Part Number: TPS563231 Dear Specialists,
My customer is considering TPS563231 and has a question about inductance value.
I would be grateful if you could advise.
---
According to the datasheet P.14, Recommended values for inductance and output capacitance…
Part Number: TPS563231 Dear Specialists,
My customer is considering TPS563231 and has a question.
I would be grateful if you could advise.
---
Regarding TPS563231, the reference voltage (VREF) are specified both minimum and maximum values at 25°C.…
Part Number: TPS563231 Hi Team,
I am curious about the input voltage and output voltage of TPS563231;
Why the device cannot work if it exceeds input range 4.5 ~ 17V range ?
Why can only output a voltage of 0.6 ~ 7V? If the feedback of the regulation…
Part Number: TPS563231 Happy new year! Wish you all the best this year.
We used the TPS563231 chip for all power regulators except High Voltage this time.
However, it seems that this chip consumes a lot of currents when it operates in the early stages…
Part Number: TPS563231 Hi.
i design circuit with this product from 12V to 5V.
but the output is not stable.
in full load the output is 4.4V and in min load is 10V
i dont know why i am having this behave.
do you have any idea?
below is my schema.
Part Number: TPS563202 Other Parts Discussed in Thread: TPS563231 , Hi team,
My customer is considering TPS563202 for temporary p2p switch from TPS563231 due to delivery shortage. Could you help us to address the questions below?
1. Could you let me know…
Part Number: TPS563231 Hello,
I'm using PSpice for TI to evaluate TPS563231. The circuit uses the reference design as it is. I checked the voltage from BST to SW. Although it is described as max5V in the data sheet, it is about 6V in the simulation. …