Part Number: TPS566238 Hi team,
I use Webench to simulate customer's application but I have one question about duty cycle simulation result.
Please clarify which portion I missed!
condition 4.6V~5.5V input and 4Voutput.
Please see 5.05V input we got…
Part Number: TPS566238 Hi,
My customer wants to simulate Signal Analysis of EN pin on TPS566238RQFR . Is it possible to release IBIS model of EN pin? If difficult, could you please let us know the RLC value of e quivalent circuit ?
Thanks and best regards…
Part Number: TPS566238 Other Parts Discussed in Thread: TINA-TI Hello,
I am having issues modeling this device in TINA-TI using the following parameters:
Vin = 4.8-5.7V
Vout = 1.9V
Iout = 2A
These are the errors I am receiving:
Irregular circuit
Component…
Hi Takumi,
For the Mode resistors, it is recommended to use the 1% resistors. I would try to keep within that range to ensure no overlapping in Modes
For the SS time. It is similar to the TPS566238. per the datasheet "The device tracks the lower of the…
Hi Moheddin
I did as you suggested and Webbench came up with the same converters as I had already found - this is the TPS566231 or TPS566238. What's your opinion on these?. My only concern is availability (or lack of)
thanks
Other Parts Discussed in Thread: TPS566238 , TPS82130 , TPS62903 Hi team
Could you help give a solution for this application?
Vin=3.3V
Vout=-3.3V
Iout=1.5A
Small-size solution
I first think of two devices: TPSM82130 and TPS566238, but
TPSM82130 output current…
Young, thanks for helping to reply.
Hi Alex,
(1) No. It can't support two 5V rail with its definition. As shown in the first page of datasheet, the adjustable range of output voltages are +/-10% based on 5V and 3.3V.
(2) That's not the recommended…
Hi Ishiwata-San,
We had a discuss with our product expert and found that device TPS54425 will not regulate vout well for above mentioned input condition.
Alternatively we recommend devices TPS565201,TPS565208 and TPS56623x(TPS566231,TPS566238) for above…