Part Number: TPS568231 Hi team,
My customer wants to set Vout=0.9V with TPS568231.
Howver, 0.9V is not listed in Table 8-2 (Recommended component values) in the datasheet.
Could you let me know the recommended values?
Regards,
Itoh
Part Number: TPS566235 Other Parts Discussed in Thread: TPS568215 , TPS568236 , TPS568230 , TPS568231 Dear Team,
Do we have suitable solution can replace MP8770CGQ?
Thanks a lot.
Jimmy
Hi Jimmy,
Yes the TPS56623x has either PG or SS. Both functions are not available at the same time. TPS56624x can be used with internal SS time of 1.39ms typ with PG feature. It looks like you need a device which has both PG and SS features available…
Other Parts Discussed in Thread: TPS568215 , TPS62136 , TPS62135 , TPS56C215 , TPS568231 , TPS568230 , TPS565242 HI ,
I am looking for alternate for TPS568215 with 4.5V-17V input and 4 A output current.
The out voltage =3.3V
Looking Efficiency and load regulation…
Hi Juliette,
Is there any method to get VFB tolerance from VOUT tolerance?
Some VRMs like TPS568231 provide the maximum and minimum value.
By using same parameter, this would be easier for us to check.
Regards,
Joey