Part Number: TPS56837 Hello team,
I would like to set the switching frequency of TPS56837RPAR to 800kHz and ILIM=7.2A. According to datasheet Table 6-1. MODE Pin Setting, 102kΩ is required. Is there no problem with this combination of 100kΩ + 2kΩ resistors…
Part Number: TPS56837 Hello team,
My customer would like to use TPS56837 with 24Vin -> 12V / 4A output. But this device is designed for output up to 13V. Is it safe to use in 12Vout configuration?
I think the minimum ON time and minimum OFF time for…
Part Number: TPS56837 According to TPS56837 datasheet, the output voltage range is 0.6-13V. What is the reason why the maximum output voltage is limited to 13V?
If the load current is small, can the maximum output voltage exceed 13V?
Hi Sean
It's nice to see Cin and RFB_bottom are close to device. (Cin can be even closer if place on the same layer with TPS56837)
The RFB_top should also place close to device other than Vo. The FB1 trace is long and is susceptible to noise. You…
Part Number: LMR50410 Other Parts Discussed in Thread: TPS56837 Hello team,
Can we measure Soft start time of LMR50410 as same as TPS56837?
I read the below document, but it requires SS pin...
Understanding Soft Start of TPS56837: https://www.ti.com/lit…