Part Number: TPS56C215 Hello,
I'd like to know about performance of TPS56C215's PGOOD pin.
What's the Max leakage current of the PGOOD pin when it's off?
What's the Max R ON of the pin's internal FET?
Best regards, Shinichi …
Part Number: TPS56C215 Hi,
Please find the following table for i/p voltage ,o/p voltages and Iout value.
switching frequency is 800Khz , i am not able to select inductor value since the webench tool and datasheets values are conflicting.
can you recommend…
Part Number: TPS56C215 Hello,
TPS56C215's data sheet describes the need for a 4.7-µF bypass capacitor on VREG5 pin, but what kind of impact can it have when no capacitor is put on the pin?
Is the 4.7-µF capacitor just a bypass one? Or, does…
Part Number: TPS56C215 Hi team
this is my customer SCH could you help me to review it ?
because I will LOA next week
can you reply this week?
there are
one TPS56C215 in page1
total 1
in attached files
BRs
brian
6036.New_schematic_Power_20230309_B…
Part Number: TPS56C215 Hi
When the load is 10A, this chip will always protect itself due to overheating. Is there a recommended way to dissipate heat?
Input/Output Voltage >> IN: 12V OUT: 3V/10A
IC and inductor temperature >> about 80 degrees…
Part Number: TPS56C215 Other Parts Discussed in Thread: TPS54628 , TPS56C231 Dear team,
Customer use TPS56C215 and design enable signal voltage level at 1.23V. Now faced to some issue if our device threshold voltage is 1.3V which is to equal datasheet…
Part Number: TPS56C215 Hi,
I can’t find the efficiency of 5Vin in TPS56C215 datasheet.
Could you please provide the efficiency data for below condition:
5Vin to Vout 1.2V@400kHz
5Vin to Vout 1.2V@800kHz
5Vin to Vout 3.3V@400kHz
5Vin to Vout 3.3V…