Part Number: TPS56C215 Other Parts Discussed in Thread: TPS568215 Hi Expert,
Due to supply shortage issue, we are proposing the TPS56C215 replace the TPS568215 now.
Pls advice the derivations between them.
And the customer point out why the Output voltage…
Part Number: TPS56C215 1V_design.docx
We have a conducted emission noise on our power cable due to 1V regulator – 1.2MHz.
We want to check the other modes to see the influence: 400KHz & 800KHz. (see DS page 16).
Is it acceptable as EyeQ4 1V…
Part Number: TPS56C215 Hello,
I am using the TPS56C215 buck regulator and after simulation, I am facing a bug in the model.
The schematic :
The simulation :
The problem is that P_GOOD2 (yellow) pin is "HIGH" when the output (pink) start risi…
Other Parts Discussed in Thread: TPS56C215 Hi
TPS56C215 is unstable in transient test.
How can I make it stable?
Transient setting:
Current:4~8A
Frequency: 1k Hz
Duty: 50%
The waveform is as below
SCH:
Thanks
BR
Hank
Part Number: TPS56C215 hi
in Equation 1
should I check any thing ?
I can caculate fp, but I don't know the next step?
is there any information can share for mye?
Part Number: TPS56C215 Hi TI,
How to check layout from ESD interference? For ESD test, I don't see any IC damage but some devices failed. First, we need to check power quality and layout, Could you please provide key point view for layout concern? Thanks…
Part Number: TPS56C215 Hi support team.
I received some questions from my customer about power-up sequence for TPS56C215.
1. Whitch correct the delay time of VREG5 to MODE is 100us or 200us?
2. If 200us is correct, why did the read start delay time from…
Part Number: TPS56C215 Dear Sirs,
May I know is there any design concern about the Rlower value in the voltage divider of FB pin?
In the datasheet and EVM user guide, the suggested Rlower(or Bbot) was fixed to 10K.
May I change it based on my design request…