Part Number: TPS60150
Hi
My Customer has question.
The customer says it can not be adopted unless the contents of the question clear. Please give priority to this question and respond.
1.In the data sheet of TPS60150, Co min = 2.2 uF is stated. This effective…
Part Number: TPS60150 Hi
My customer has question.
The customer wants to turn ON/OFF the TPS60150 with a signal to turn ON/OFF the LED of the load. (Request specification on the load side) ON / OFF is scheduled to be performed with a signal of maximum…
Part Number: TPS60150 Hi
My Customer has question.
■Q1 Although the TPS 60150 has the Short Protection function,Do you also have Current limit Protection function? Is it possible to understand that the threshold is 300 mA from Datasheet P10 Figure 6?
■…
Part Number: TPS60150 Hi
My Customer has question.
When Ta = -10 ° C, the ripple voltage is disturbed. Are there any possible factors?
TPS60150.pdf
Best Regard
T Kishi
Part Number: TPS60150 Other Parts Discussed in Thread: TPS65150 Hi
My Customer has question.
TPS65150 is there no problem if voltage remains at 5V ,in the absence of Vin?
Customers are worried that problems will not occur when the input voltage runs out…
Part Number: TPS60150 Hi
My Customer has question.
TPS60150 has dischrge circuit?
■customer SPEC
VIN=3.3V
VOUT=5.0V
IOUT=9mA
Load:LED
If the output voltage does not decrease at no load, we are worried about the problem.
Best Regard
Part Number: TPS60150 Hi,
My client has a question about TPS60150.
Q.How much is the soft start time variation?
If you have any information, would you please tell me.
Thank you.
Other Parts Discussed in Thread: TPS60150 Hi,
Please teach me skipmode switching frequency range of TPS60150.
I've read [The skip threshold voltage and current depend on input voltage and output current conditions.] in the datasheet(rev.B) P11.
But…
Other Parts Discussed in Thread: TPS60150 Hi,
We are planning to use TPS60150 charge pump in our design.
our question is, whenever chip is in disable state [Enable=low] if we apply voltage to the Vout pin[ 3.5V to 4.2V] will there be any damage to the chip…
Other Parts Discussed in Thread: TPS60150 , TPS61220 Hi,
May I know whether TPS60150 can be used for my application which
requirement as shown below:-
a) Vin = 2.9V to 4.2V
b) Vout = 4.8V ~ 5.5V
c) load current = 3uA ~ 10uA
My concerns here when I select…