Part Number: TPS60400-Q1 I would like to ask about 8.3.1 Charge-Pump Output Resistance in the datasheet.
What is the value of R_SWITCH in Equation 1, which is the formula for R_O?
Part Number: TPS60400-Q1 Hello team,
TPS6040x has several variation, fixed Fsw or adjustable.
What's the benefit of fixed frequency? Is there any application reason of each 20k/50k/250kHz ?
ti
Part Number: TPS60400-Q1 We are using the TPS60400QDBVRQ1 inverter now in one of our product type in my company.
This is a product that has an operating temperature of -40 degrees to +125 degrees.
We now want to use this inverter for a new product…
Part Number: TPS60400-Q1 Dear All, I am trying to generate a -3V thanks to the TPS60400Q1 device, in a system I designed However, when I power on the system (Vin = 3V), it generate a -0.8V, that drops to -0.3V after a few seconds
Please find below the…
Part Number: TPS60400-Q1 Other Parts Discussed in Thread: LM2776 , SN74LVC1G14-Q1 Hi Team,
The recommended operating voltage is 5.25V, and the max is 5.5V. Is there any concern with operating this at 5.3V.
Application 5.3Vin -> -5.3Vout
thank you…
Part Number: TPS60400-Q1 Other Parts Discussed in Thread: TPS60400 The whole vehicle CAN has no communication, and the analysis down is this chip on the board: chip failure: pin1 & pin4 voltage drop value is abnormal, caused
Part Number: TPS60400-Q1 Other Parts Discussed in Thread: TPS60400 , TPS60140 , REG710-33 , SN74AHCT1G08 We would like to make a 3.3V-5V power supply by boosting from the LDO output power supply of about 2.5V, 40mA. I would like to use Charge Pump Power IC…
Part Number: TPS60400-Q1 Dear team,
In our datasheet, there is one parameter named VACeff as below, but there is no definition about this. Could you please tell me what does that mean?
Thanks & Best Regards,
Sherry
Part Number: TPS60400-Q1 Other Parts Discussed in Thread: TPS60400 Hi, team.
Is the maximum rating of OUT to GND of TPS60400-Q1 -5 V, is it correct? Is it -5.5V?
Best Regards,
Part Number: TPS60400-Q1 Hello Team,
Do we have any information about what the output impedance of the TPS60400-Q1 looks like when the input voltage is below 1.8V?
The graph on page 7 of the datasheet seems to show it going to 35ohms and probably higher…