Part Number: TPS61032 I'm using the TPS61032PWPR in a new design. Input: 5V DC after diode V drop: 4.5-4.8V Battery: 3.0-4.2V
Since I'm using the TSSOP package the layout is based closely on the TPS6103x EVM-208 datasheet in addition to the TPS61032…
Part Number: TPS61032 Hello,
I am designing a new board, where I need to have a stable 5V output. The load will be around 100 mA with spikes up to 1,3 A for approx. 10 milliseconds (Iridium 9602 module). The voltage drop during the spike should not be…
Part Number: TPS61032
Hi everyone,
I have just soldered a new PCB with TPS61032. All seems good, except the TPS61032 not turning off when EN pin is grounded (it is always on, does not matter what is the status of MCU pin (high-low). The EN pin is controlled…
Part Number: TPS61032 Hi , I made a design for the TPS61032 to power up the Arduino Nano and the SG90 servo. The TPS61032 seems unable to power the servo. It is suppose to generate 1000mA at 5V but I seem to stall at 200mA at 5V.
Please help,
Andy
Part Number: TPS61032 Hi TI, I have made a low battery indicator light using the TPS61032. but the light seems to slighty turn on as the battery is getting drained. The voltage is currently 2.5V and the design value was 2V and the low battery light is…
Part Number: TPS61032 Other Parts Discussed in Thread: TPS61030EVM-029 , TPS61023 , TPS61030 Hi, With reference to the Case CS0634034 and CS0558572 here is my updated design. I request you to have a look at the layout. I tried to match it with TPS61030EVM…
Part Number: TPS61032 I have concern Switching frequency of TPS61032 interfere AM radio band. Could you advice how to resolve EMC issue? for example, snubber circuit, shield, filter, etc
Part Number: TPS61032 Other Parts Discussed in Thread: TPS61022 I'm trying simulation of Power Designer.
Following is my setting. (input voltage:3.0V-4.6V, output voltage:5.0V, output current:3.0A)
But it is appeared error below.
Could you tell me…
Part Number: TPS61032 Other Parts Discussed in Thread: TPS61030 Hi team,
I'm looking at using the TPS61032 as an alternate to the TPS61030 in the QFN package. Am I okay to place the TPS61032 on the board and leave the feedback resistors, that I had been…
Part Number: TPS61032 The actual part number of the part is
TPS61032RSAR
Kindly do a detailed review of the Boost section. The component details and the schematics were attached below.
So please compare the c omponent features matching the boost…