Part Number: TPS61041-Q1 Hi TI-team
My customer have question.
Please tell me the MIN value of the absolute rating of Switch voltage on pin SW.
MAX=30V.
MIN=???
Best Regards,
Koji Hayashi
Part Number: TPS61041-Q1 Dear TI:
Custom use tps61041-q1 to output multi channel voltage including positive voltage and negative voltage. input voltage: VCC=3.3V. Output voltage= ±5.6v, 16v,-15v。。 small output current.
can ti help to check the following…
Part Number: TPS61041-Q1
Hi TI-team
1:Is it possible to apply 10mA to each terminal from the GND terminal ?
Is there a possibility that the IC will be damaged ?
Also, can you guarantee on all terminals after this test ?
IC assumes non-energization…
Part Number: TPS61041-Q1
Hi All
How does it affect the output voltage when operating between the maximum recommended voltage and the absolute maximum rating ?
Also, are there any other Electrical Characteristics that affect ?
Best Regards,
Koji Hay…
Part Number: TPS61041-Q1 Hi All,
What is the resistance value of RSENSE ?
Is it included in the resistance value of Datasheet's Ron ?
Best Regards, Koji Hayashi.
Part Number: TPS61041-Q1 Other Parts Discussed in Thread: TPS61040-Q1 Hi All,
There are efficiency results in Fig.1 to Fig.4 of the data sheet.
Please tell me the BOM when you measured.
Best Regards, Koji Hayashi.
Part Number: TPS61041-Q1 Other Parts Discussed in Thread: TPS61170 Hi All,
Is it OK to connect to SW and VIN with different voltage?
(12V-Coil-SWpin)
For example, VIN = 6 V, SW = 12 V
Is it OK if the absolute maximum ratings are observed?
Customer's expected…
Part Number: TPS61041-Q1 Hi All
My customers are concerned about noise due to switching frequency.
Is there a graph or calculation formula showing the relationship below?
1,Switching frequency vs output current.
2,Switching frequency vs ambient temperature…
Part Number: TPS61041-Q1 Hi All,
What happens when FB is shorted to GND?
Is the IC broken?
I think that the output voltage rises and exceeds the withstand voltage of the SW pin.
Best Regards, Koji Hayashi.
Hi Helen-san
How is the state of progress after that ?
When can I obtain measurement results ?
Customer is in the process of examining whether to use TPS61041-Q1.
There are additional evaluation conditions. Vin=3.56V Vout=20.21V Iout=3.09mA,7.14mA
First…