Part Number: TPS61087 Hello, guys.
I can't get the Spice model for TPS61087 to work on LTSpice. I'm only using the circuit showed in product's datasheet. Could anyone be able to help me?
Thank you,
Part Number: TPS61087 Hi Team
I would like to request a check of the circuit diagram of the TPS61087, so would it be possible for us to communicate via e-mail?
We would like to keep the circuit diagram private, so please consider this.
Best Regards
Part Number: TPS61087 We are conducting actual machine verification using the circuit on the next page.
As a result, boost operation may stop when Iout=1.0A.
At this time, the coil makes a noise.
There was no problem with WEBENCH, but could you please…
Part Number: TPS61087 Hi,
I have to design a Boost converter for 650kHz.
Required Specifications are listed below.
Input Voltage range is 2.7-4.2
Nominal 3.7V
Output Voltage 12V
Current 367mA
The Boost design in datasheet shows an inductance value of…
Part Number: TPS61087 Hello
Thanks for the schematic review feedback.
Kindly review the layout file and give us your valuable feedback as soon as possible.The designator in layout for the TPS61087 is U3
4188.[3] POWER.pdf A4415-A00-PCB_Gerber.rar Please…
Part Number: TPS61087 Hello
We are using TPS61087DSCR in our design .Please review our design and give us your valuable feedback as soon as possible
Kindly find the attached 3122.[3] POWER.pdf schematic pdf
Part Number: TPS61087 Other Parts Discussed in Thread: , TPS61169 Dear team,
My customer are trying to develop TPS61087 for LED supply. but there is issue of audible noise under PWM operation.
When they input 100% PWM, there is no audible noise but if…
Part Number: TPS61087 Hi,
We are using the part TPS61087 in our design for a 5V to 12V boost converter with a current limit of around 1A. But, whenever we are trying to increase the load greater than 300mA, we are observing a voltage drop in the 12V rail…