Part Number: TPS61093 Other Parts Discussed in Thread: TPS61089 , , TPS61372 , TPS81256 , TPS61085 I am looking for a DC\DC regulator with following requirements :-
Vout = +12V, Vin = +5V Iout = 0.5A aprox.
I am looking for the smallest PCB area !
One of…
Part Number: TPA6120A2 Other Parts Discussed in Thread: TPS61093 I'm using a TPA6120A2RGYT as a headphone audio amplifier. The application is battery powered and I have a TPS61093DSKR generating +/-12V for the amplifier.
I've prototyped the amplifier…
Part Number: TPS61093 Dear Support team
We can find Start up waveform in Figure 17 datasheet of TPS61093. I guess the startup time will be 184ms at Figure17. Since the capacitance connected to SS pin is 1uF, tss softstart time will be 100ms. I know tss…
Part Number: TPS61093 I have a TPS61093EVM evaluation board from TI, as well as a custom made PCB featuring this part in an embedded application. Both the EVM as well as the custom PCB are suffering from fairly extreme excursions in the transient response…
Part Number: TPS61093 Dear Team,
Please tell me the start and end conditions of the SS time in Equation 2.
Is the start point defined as EN=H?
What is the end point defined as?
Best Retards,
Hirokazu Takahashi
Part Number: TPS61093 Hi Team,
May I connect VO and OUT?
< Background>
According to “8.1 Overview” of the datasheet, “However, shorting the VO and OUT pins bypasses the isolation switch and enhances efficiency.”.
Therefore…
Part Number: TPS61093 My customer would like to check if they could remove the R3/C5 which connected to SS pin for soft start control if there is no specific SS time requirement in their design? They would like to use in very space limited design. Please…
Part Number: TPS61093 Other Parts Discussed in Thread: TPS61085 Tool/software: WEBENCH® Design Tools Hi,
We is thinking about using this device below condition. Vin:5V Vout:8V Iout:0.5A
But this device has Overload protection. This threshold value is Typ…
Part Number: TPS61093 Dear support member,
My customer used TPS61093.
I have a question.
Could you teach Isolation FET on-resistance charactice graph? ( Horizontal axis Vout vs Vertical axis on-resistance graph)
Best regard. Bob Lee.
Part Number: TPS61093 Hi Team,
Our customer would like to know the scatter plot of Vref.
We understand that the min/typ/max values of Vref are is mentioned in datasheet.
However, they would like to know the scatter plot of the average value and standard…