Part Number: TPS61096A Dears currently used TPS61096A for variable output application through switching dedicated resister divider using external - mosfet ,
so couly you help check below parameter may related with my application
1. Vosns - output voltage…
Part Number: TPS61096A Other Parts Discussed in Thread: TLV61046A HI TI expert,
I have the requirements as below:
Vin=2.5~3.3V
Vout=12V
Iout max=80mA
TPS61096A is selected for our design to meet the above requirements.
But when I try to generate the schematic…
Part Number: TPS61046 Other Parts Discussed in Thread: TPS61096A Hi team,
Could you help check if we get the following boost part recommendation?
Number of Output
VIN
VOUT
IQ
ILoad
1
2V ~ 3V
8V
28uA Max.
5mA Max.
Thanks and…
Part Number: TPS61096A Hi,
I have two questions related to level shifters.
1. When device is disabled (EN=0V) and LVIx is logic high, what would be level on HVOx?
2. Electrical specs on page 5 list level shifter sourcing and sinking current to be 800uA…
Part Number: TPS61096A Hi
From the functional block diagram of the TPS61096A I can see there is a FET between VOUT and VOSNS. I am assuming this is used to disconnect the feedback network when the device is disabled to reduce leakage current? However…
Part Number: TPS61096A Other Parts Discussed in Thread: TPS61096 Tool/software: WEBENCH® Design Tools Hi Team,
we'd like to use Tina to simulate the total input power of the circuit.
Please kindly check attached. it takes 2ms for the part to be in…
Part Number: TPS61096A I'm running a lightly loaded TPS61096A with a 6.5V output voltage. R1 and R2 in the feedback network are 10k and 1.82k. I don't see a very steady voltage on this pin. It looks more like a square wave. I'm not sure why it…
Part Number: TPS61096A Tool/software: TI C/C++ Compiler Tps61096a user manual design access circuit, can not output the specified voltage, and the current consumption greatly fluctuates 0.5mA~20mA
Part Number: TPS61096A Hello,
What is the functionality of VOSNS pin in TPS61096A boost converter. Is it for remote sensing for taking the feedback from load?
Please explain what it is and what are its functionalities / advantages? Thanks in advance. …