Part Number: TPS61165EVM-283 from this link https://www.ti.com/tool/TPS6116XEVM-SW I am unable to install software on my device. I have a system that is compatible with the software. Let me know the steps to install the software on my device. I hope if I…
Part Number: TPS61165EVM-283 I bought an EV board called TPS61165EVM-283 and the dimming mode is not working.
Everything is powered up and the LEDs are on full brightness this is the error we're getting on the GUI even though the USB is lit up green…
Part Number: TPS61165EVM-283 We purchased this development board, the official website saw that there is a matching disc, but we received the goods are not, this development board factory accessories have no matching disc.
Part Number: TPS61165 Hi team,
I have to bring up TPS61165EVM-283 backlight driver with IMX8MM-evk NXP processor in android 11 code base.
As of now i have made changes in following files:
drivers/video/backlight/Kconfig
drivers/video/backlight/Makef…
Part Number: TPS61165EVM-283
Hi,
I am using the TPS61165EVM to drive an LED bar that is external to the module. The TPS61165EVM is designed for an input voltage of 5V ± 10%. I would like to use a different range, from 3V to 7V. Which components should…
Part Number: TPS61165EVM-283 Downloaded and installed the software from the link in the user's guide. Running with power supply, software only allows me to enable/disable the chip. Any change to the FB register results in "no ACK" from device, and no…
Part Number: TPS61165EVM-283 Hi,
We're using TPS61165's EVM for an evaluation under the following conditions:
Vin,typ = 3.3V
Vout,max = 21V (for 1 string of 7 series-connected WLEDs)
Iload,max = 65mA (i.e. Rset ~ 3 ohm)
PWM dimming via CTRL …
Part Number: TPS61165EVM-283 Hello all,
I just received the TPS61165EVM-283 Eval Module. I installed the driver and then plugged in the USB Adapter and then attached it to the TPS561165 demo board.
The software does run but it says its not connected to…
Part Number: TPS61165EVM-283 I've disconnected JP2 on this eval board, and soldered a wire across J4 so I can connect my own LED array across J3 and J4. My array consists of twenty-four OSRAM 4240 in series.
I'm seeing two different unexpected occurrences…
Part Number: TPS61165EVM-283 Dear all
I just bought the evaluation kit and tried to used it with the easyscale protocol enabled. The onboard LEDs do not change brightness however.
Here is what I did
a) The CD delivered with the kit, is empty. I hence…