Part Number: TPS61196 Hi Ti engineer,
Our schematic diagram is as follows. There will be overshoot as shown in the starting process. Would like to ask how to remove this overshoot
Part Number: TPS61196 Hi,
The customer is using TPS61196 for LCD backlight.
After production, the screen shook in the 50% brightness test.
One to two occurrences in 100 production: If you change TPS61196, the screen shaking will disappear.
Can you advise…
Part Number: TPS61196 Hi,
We have a backlight driver IC requirement for AUO make panel. Below is the panel specification. I have used TPS61196 backlight driver IC. I am giving 200Hz PWM signal and using 6 channels.I have changed the VOVP threshold value…
Part Number: TPS61196-Q1 TPS61196-Q1 drives 6 street lamp beads, 4 of which are connected with 16 lights in each road; The other 2 roads are connected with 17 lights each. Can they work normally?
Part Number: TPS61196-Q1 Five of them are used in tps61196-q1. If there is one street lamp with less beads than the others, can it work normally? (21 lights for 4 roads, 14 lights for 1 roads)
Part Number: TPS61196 Hello
I am not using the UVLO function of the TPS61196, as per page 13 of the datasheet, I intend to pull the UVLO pin to VDD pin of the TPS61196. Should this connection be direct, or through a pull-up resistor? If a resistor should…
Part Number: TPS61196 Hi,
I'm trying to test the evaluation board using an Arduino Mega to proide the PWM signal for dimming the LEDs (connected to only one output channel), but as soon as I connect the PWM input to the evaluation board, I get a FAULT…
Part Number: TPS61196 Hi,
We have a AUO make LCD panel which require LED Backlight driving IC. We need 6 channel LED back light driver and each channel will require 43mA current maximum. LED forward voltage is 110V maximum. Input voltage available in…