Part Number: TPS61196EVM-600 Other Parts Discussed in Thread: TPS61196 Dear Support,
I am using Tps61196 as role model to design my PCB. I have a question of the PCB layout out of TPS61196. from high voltage output to ground for example cross C4, or J3…
Part Number: TPS61196EVM-600 Dear Support,
I have a simple but hard to answer question. on the demo board of
TPS61196EVM-600.
I don't see the ESD protection on the connector J3, which connector U1.12, 13, 14, 15, 16, 17 to the external world. I trust…
Part Number: TPS61196EVM-600 Dear TI support,
is it possible to get a TPS61196EVM-600 schematic in Orcad format. it will save a lot of time for me to input all the parts/symbols.
Thank you very much,
David
Part Number: TPS61196EVM-600 Other Parts Discussed in Thread: TPS61196 Dear Support,
I have a TPS61196EVM-600, I am going to modify the board to make output to 350mA at 80V. here is my calculation.
1. Iset = 350/4992 = 87.7uA.
2. R11 = 1.229/87.7 = 14K…
Part Number: TPS61196EVM-600 I need the 400mA design on my setup. I have changed R26 (ISET, 37.4K, 130mA) to 12.3K ( I believe it will make 400mA) based on ILED(400mA) =VISET(1.229)/R26(12300) x KISET(3992). Actually I fed 5% duty 60Hz PWM, and changed…
Part Number: TPS61196EVM-600 Hello,
My customer needs the following trade compliance info for TPS61196EVM-600 :
US Harmonized System (HS) Code:
Export Control Classification Number (ECCN):
Thank you, Alan
Part Number: TPS61196EVM-600 Other Parts Discussed in Thread: TPS61196 Hello team,
My customer is evaluating TPS61196 with using its EVM. However customer saw fault signal and couldn't operate the EVM.
For the measurement, they modified below points…
Part Number: TPS61196EVM-600 Other Parts Discussed in Thread: TPS61196 , , LP8556 I have attempted to modify a TPS61196EVM-600 to support two strings of 20mA LEDs but the TPS61196 does not appear to be starting up. I do not see any switching of the switching…
Part Number: TPS61196EVM-600 Hi
Please let me ask you about TPS61196EVM-600?
Could you tell me the following questions?
・Dimension of EVM
・Dimension and position of screw
Best regards,
Yokota