Part Number: TPS61235P Hello. I'm planning to use a TI TPS61235P boost converter IC for an upcoming project (VOUT 5V/3.5A with a VIN_min of 3V). In the features TI mentions there are two 10A internal power switches for the synchronous function but in…
Part Number: TPS61235P Hi,
My setup including TPS61235P, BQ27441 Fuel Gauge and 18650 3500 mAh Li-Ion Battery.
When my load is 5V 2A, the battery current is rising 3A . (Battery voltage= 3.6V) . I am getting battery current value from Fuel Gauge.
These…
Part Number: TPS61235P Tool/software: WEBENCH® Design Tools Hello Guys,
Good day.
Our customer is trying to export the CadSoft EAGLE file for TPS61235PRWLR but keeps encountering "Export Failed". He already tried on Chrome and Edge but was unable to do…
Part Number: TPS61235P Other Parts Discussed in Thread: BQ25895 , PMP4451 , PMP11536 Hi,
In reviewing the PMP4451 reference design, I see that TPS61235 is used to boost the output of BQ25895 to 5V3A. However, BQ25895 already has a built-in boost converter…
Part Number: TPS61235P Hi Team,
I found that the TPS61235's min Vin is 2.3V。
If the input of TPS61235 is less than 2.3V, it will trigger to UVLO,right?
When in UVLO status, will the TPS61235 shunt down? What is the input current or current consumption now if…
Part Number: TPS61235P Hi,
I can only get 1.2A output current before a protection happening, and after that ,the output can only have about 2.2V output voltage. When I touch the chip, the temperature is not high. And I can ensure the Vin is always 3.3V…
Part Number: TPS61235P Hi!
In my project, a circuit with two power boost Dc-Dc converters TPS61235P. Ground is common. The power circuits are connected to a common point to which different loads are connected. Is it necessary to use diodes between two…
Part Number: TPS61235P Hi:
I am currently designing a power supply using TPS61235P. I have a question related to the Enable pin. Could i tie it to the VIN pin in case of not using it ?
Thanks