Part Number: TPS61236P Other Parts Discussed in Thread: TPS61022 Dear TI Team,
If the difference between the input voltage and the output voltage of the TPS61236P is designed below 0.5V, can you know what kind of damage it does to the IC?
VIN: 4.2V Vout…
Part Number: TPS61236P Other Parts Discussed in Thread: BQ24773
Above is a scope of the startup of boost based on the TPS61236P. the circuit quickly rises to the input voltage. Hangs there about 8 seconds and then slowly begins to rise to the 5V…
Part Number: TPS61236P Tool/software: WEBENCH® Design Tools Hello,
I try to create a custom inductor in the Webench, but I realize that after creating and saving the new part, Some parameters are not shown in the inductor list (like: Irms, Tolerance,…
Hi Danilo,
Sorry, where is PTC and its effect on short Vout? I did not see it in PCB. and how did customer short Vout, through Cout or directly short IC Vout pin?
Maybe can short C17 or C25, or even directly short C25/C17 Vout pin and GND vias, which is shown…
Part Number: TPS61236P Other Parts Discussed in Thread: TPS61022 Hi. Attached is the concept I came up with for a 5V output boost converter using the TPS61236P. Can someone help review this? In this application the boost converter can be turned on by…
Part Number: TPS61029-Q1 Other Parts Discussed in Thread: TPS61236P Hi,
Is there Web bench design available for this convertor? Also can you please suggest any automotive alternate part is available for this part which is having web bench design available…
Part Number: TPS61236P Hi,
I have built a li-ion to 5V @ 4A constant current DC converter using TPS61236P (the circuit and most of the resistor and capacitor values come from WEBENCH while some changed a little) but it turned out that the output can't…
Part Number: TPS61236P Dear Sir,
My system is very important efficiency of boost converter for TPS61236P.
Inductor is 0518CDMCC of SUMIDA.
=======================================
Setting value :Vin: 3.7V , Vout: 5V , Iout: Max 2.5A
=================…