Part Number: TPS61236P Hi Team,
Our customer want to use Vin=4.7V to have 5V output by TPS61236P.
Based on datasheet, it request 0.6V gap.
What will happen when Vin too close to Vout?
Thanks
Shaq.
Part Number: TPS61236P Dear TI team,
I have a question if TPS61236P would be possible for me to achieve my goal.
I have an LDO voltage which would be an input voltage (3.3V, 80mA) and I want to boost it to get an output voltage of 5V, and, with an output…
Part Number: TPS61236P Dear support member,
My customer used TPS61236P. This project is urgent.
(Situation) Regulator TPS61236PRWLR, but we are currently implementing it in our prototype and checking its operation.
Voltage etc. are output correctly, there…
Part Number: TPS61236P Other Parts Discussed in Thread: TPS61253A , TPS61022 , BQ24073 Hello,
I read the related post https://e2e.ti.com/support/power-management/f/196/t/757404 and I too have this issue with audible noise. I measured the voltage at the input…
Part Number: TPS61236P Other Parts Discussed in Thread: TPS61236EVM-676 Hello TI Support,
I am working on a design that has the TPS61236P. I have set the output using resistors R1/R2 to be 4.9V. The input voltage is 3.7V.
I am using an electronic load…
Part Number: TPS61236P Dear all:
I used TPS61236P for 3.7-4.3V to 5V/1A. We test efficiency of lignt load is not meet DATASHEET. Can you help to solve the problem?We need about 90% efficiency , thanks!
Vin
I(input)
Vout
I(output)
效率…
Part Number: TPS61236P Dear Sir
TI Part Num: TPS61236PRWLR (PKG type: VQFN-HR_RWL-9pin) I would like to confirm if the recommended operating junction temperature maximum is 125 degree C, or not.
Datasheet describes as below. 7.3 Recommended Operating C…
Part Number: TPS61236P What is the start up time specification from when the EN pin goes high to when output reaches nominal voltage level?
Thanks,
Ken
Part Number: TPS61236P Other Parts Discussed in Thread: TPS61230A Hi, Could you tell me about the dynamically variable output voltage of TPS61236P? Customer wants to change the output voltage by applying voltage to the FB pin. Connection configuration is…