Part Number: TPS61288 Is there an efficient way to connect two of these circuits in parallel for more output current. My situation is 7.2V in, 15V out. I see this question has been asked a couple of times before, but the answers were taken to private…
Part Number: TPS61288 Tool/software: I am using the TPS61288 to take in a variable input between 3.5- 4.5V at a max supply of 5A and intend to step it up to an output of either 5V, 9V or 12V; I expect a peak current draw of 2A for a 12V load. Basically…
Part Number: TPS61288 Tool/software: Hi, TI expert
I would like to request a schematic review of TPS61288. The specifications are as follows:
- Input Voltage : 3.6V~4.2Vdc (Use battery)
- Output Voltage : 13V~16Vdc
- Output Current : about 10A…
Part Number: TPS61288 Tool/software: Hi Team,
My customer found the output voltage is not 0V while TPS61288 disabled(EN=0)
The Vin=5.28V and Vout=12V.
While EN=1, the Vout=12.5V, but while EN=0, the output still had around 4.9V
Please help to…
Part Number: TPS61288 Hi Team,
in the block diagram of TPS61288, Vout is also connected to the internal LDO, along with Vin. I would to understand what's the design purpose for a boost converter (since Vout is > Vin, using Vout as source actaully decreases…
Part Number: TPS61288 Hi, TI expert
A customer has asked me what the body diode's allowable current is, to determine the current specification that can flow to the load when the TPS61288 is turned off.
Could you please confirm this?
Thank you…
Part Number: TPS61288 Tool/software: Hi Sirs,
My customer needs to double check whether the reverse current(current flow from output towards input) would occur or not.
They think the reverse current would happen when enable is low or Vin falls down…
Part Number: TPS61288
Tool/software:
Hi TI experts,
I notice the output capacitors in tps61288 reference circuit are 6*22uF.
If I only place 2*10uF at Vout because of the limitation in pcb spacing, in addition to increase power ripple, what…
Part Number: TPS61288 Tool/software: Hello,
My customer is looking for a Booster IC that can support the following conditions.
- VIN = 3.7V (18650 Battery)
- VOUT = 28V / 10A
If there is a TI Booster product that satisfies the above specifications…