Part Number: TPS65131 Other Parts Discussed in Thread: TPS62143 , LM5160 , PMP10733 , PTN04050C , LMZ34002 Hi Sir
My customer Vin can be 5V or 9V.
and request Vout is +/- 15V Iout 100mA. may we have suggest solution?
Another request is Vin can be 5V or 9V…
Hello Kazuki,
It seems there is a mix up between two parts on our website which will be fixed thanks to you. You are right TPS62163 does not have an output discharge function. I would recommend you take a look at the TPS62133 / TPS62143 which do have this…
Other Parts Discussed in Thread: LM5036 , TPS62143 , TPS54427 , LP5907 , TPS62130 , LP38841 , TPS56720 Here is the design that web bench designed, it suggests an LM5036 but this part does'nt exisit. Is this a typo? What woudl the part really be? webench.ti…
Other Parts Discussed in Thread: TPS62143 , TPS62140 The datasheet does not specify how to calculate the output accuracy when using the adjustable (tps62140) version with an external resistor divider. For example, the reference tolerance is sometimes provided…
Other Parts Discussed in Thread: TPS62143 , TPS62110 , TPS62142 , TPS62160 Got the below problem:
We are currently evaluating TPS62142RGT and TPS62143RGT chips.
operating conditions for TPS62142RGT : VIN=12V; FSW=GND; DEF=GND; L=2.2uH (VLS3010T-2R2M1R3) SS…
Hi,
Would the attached example be OK if I wanted to mix USB 5V (optionally plugged in) and the TPS62143? I am reffering to the diode in particular.
Use cases the solution should be able to handle:
Only battery connected: OK!
Only USB connected: OK (ignoring…