Part Number: TPS62162 Other Parts Discussed in Thread: TPS62160 , TPS629210 , TPS629210-Q1 Hi,
Good Day. I have a customer who is working with TPSM84205EAB. Please see below his query for your reference. Thank you very much.
Due to the short supply…
Part Number: TPS62162 Hi
I got two questions about TPS62162 from my customer.
Could you tell me the following questions?
1. What is the Vout accuracy at Vout≦Vin<Vout+1V?
2. Are there the data of figure 19 at Vin<4V?
Best regards…
Part Number: TPS62162 Other Parts Discussed in Thread: TPS629210-Q1 , TPS629210 , TPS62170 , , TPS62125 Hi There!
Due to shortages TPS62162DSGR is backordered until next year which is impacting production for me. I am researching alternates. Does TI…
Part Number: TPS62162 Other Parts Discussed in Thread: TPS62840 Hi
My customer would like to get the efficiency data at Vin=5V Vout=3.3V and Iout=30uA of TPS62162.
Could I get that's data?
Best regards,
Yokota
Part Number: TPS62162 Hi There!
I just wanted to double check something. I used power designer to configure a TPS62162DSGR. Essentially I am trying to achieve a vOUT of 3.3v with a max output current of 1A. This is the design it produced:
What…
Part Number: TPS62162 Other Parts Discussed in Thread: TPS62147 Hello,
I need to know what the planned lifetime for this part is before going obsolete. Does TI have a longevity program for this part?
Thanks,
Juan Martinez
Part Number: TPS62162 由于给DSP供电时,DSP老是会进入低功耗模式,所以我单独测试TPS62162DSGT产生的电压,滤波后产生电压的幅值是3.3V,幅值是正常的,可是发现TPS62162的PG端口产生的波形不是PWM模式否而是Power Save Mode这个模式,然后我改变3.3V的负载的大小,发现仍然是Power Save Mode这个模式,只不过是占空比变大了,仍然没有运行于PWM模式,请问一下,这是什么原因导致的?
Part Number: TPS62162-Q1 Other Parts Discussed in Thread: TPS62162 , , TPS62172-Q1 Hi Ti Team,
This is the part we are using for step down converter: TPS62162-Q1
Input voltage = 5 V
Output voltage = 3.3 V
Maximum required load current = 400 mA…