Part Number: TPS62260-Q1 Other Parts Discussed in Thread: TPS62260 Hi,
Could you tell me the themal Information of RθJA, RθJC(top), RθJB, ΨJT, ΨJB and RθJC(bot).
There is information on catalog product, but does not it exist…
Part Number: TPS62231-Q1 Other Parts Discussed in Thread: TPS62290-Q1 , , TPS62260-Q1 , TPS62230 , TPS62260 Hi
I got a question about the fillet from my customer.
There are written the following text attached link.
As long as I read them, I think TPS62231…
Other Parts Discussed in Thread: TPS62260-Q1 I would like to confirm the operation mode of TPS62260-Q1.
The customer conditon is below;
- VIN: 5V
- VOUT: 1.3V
- IOUT: 0.1A
- MODE: fixed PWM
In this case, does TPS62260-Q1 keep PWM mode with CCM?
I want…
Hi Keiichi,
PFM is not working with constant switching frequency. It is possible to work with switching frequency above 1.5MHz in PFM mode but TPS62260-Q1 has to be loaded.
Figure 22 in TPS62260-Q1 datasheet shows different switching frequencies for…
Part Number: TPS622314-Q1 Other Parts Discussed in Thread: TPS62260-Q1 Dear TI,
Do we have a p2p device with TPS622314-Q1? which can achieve 3.3Vout? Thanks for recommendation.
Part Number: TPS62067-Q1 Other Parts Discussed in Thread: TPS62290-Q1 , TPS62260-Q1 Hi,
intention is to use TPS62067-Q1 in following constellation:
Vin = 5v0
Vout = 3v3
Iout = 0.49A
L = 1µH
Current ripple is approx. 70%.
Is it possible to incre…
Are there any other recommended switching regulators for generating the core voltage? I have seen one application example using the TPS62260-90-Q1 and one using the TPS57112.
I was thinking of using the TPS62160 (or equivalent in SOP package) instead,…
Other Parts Discussed in Thread: TMS570LC4357 , TPS62290 , TPS62260 , TPS65381-Q1 , TMS570LS3137 , TPS57112-Q1 We are in the process of designing a product that will use the TMS570LC4357. Other TMS570 microcontrollers have a low enough power consumption that…
Other Parts Discussed in Thread: TPS43340-Q1 , TPS62260-Q1 Hello all,
I am planning to use QUAD-OUTPUT POWER SUPPLY IC TPS43340-Q1 in my new design.
My first question concerns with the use of LDO regulator on this IC. There is no 'Vdropout vs Iout' graph…