Part Number: TPS62420 Hi,
my customer is using TPS62420 and they would like to extend the operating ambient temperature range to 105C.
So I find TPS62420-Q1, but the only difference is:
We only specify TPS62420-Q1's operating junction temperature to …
Part Number: TPS62420
Hello
we designed 3.3V and 1.2V for a Delfino uC input voltages.
channel 1 is the 3.3V - we get 1.25V
channel 2 is the 1.2V - we get 1.2V
the diode D8 is to match as much as possible the rise of the voltages for the uC.
another…
Part Number: TPS62420 Other Parts Discussed in Thread: TMDSDOCK28335 , TMDSCNCD28335 , TMDXCNCD28388D , TMDSCNCD28379D , TMDSDOCK28379D , LAUNCHXL-F28379D Hello!
We have been using TPS62420 for many years in a number of our reference designs, and its been…
Part Number: TPS62420 I'm getting $CDCENCSTART when I try to import the model - downloaded from here http://www.ti.com/product/TPS62420/toolssoftware
. How do i get the unencrypted spice model?
Thanks,
Michael
Part Number: TPS62420 Other Parts Discussed in Thread: TPS62821 , TPS62840 Hello experts,
My customer is considering DCDC converter having two outputs.
Input: 3.0V
Output: 2.0V, 500mA / 1.8V, 500mA
In addition, customer wants enable these output about…
Part Number: TPS62420 Other Parts Discussed in Thread: TPS54120 Dear,
we saw C2000 reference ,power choice is TPS62420, but customer change to Vin 12v, could suggestion Suitable for C2000 power.
If any suggestion, Please advise me.
Thanks,
Best regards…
Part Number: TPS62420 My question is basically the same as this one: https://e2e.ti.com/support/legacy_forums/automotive/f/26/t/550678?tisearch=e2e-sitesearch&keymatch=tps62420%2520def_1%2520bias I'm using the TPS62420 to create 3.3V and 1.2V for a…