Part Number: TPS62421 I am using a fixed default output part (TPS62421) to generate 1.8V and 1.2V rails for a system.
I am seeing higher voltages (1.93V and 1.27V, respectively). As load increases, the voltage rises with 1.93V/1.27V being the maximum…
Part Number: TPS62421
I am using a fixed default output part (TPS62421) to generate 1.8V and 1.2V rails for a system. In certain low load scenarios I'm seeing the 1.8V output go unexpectedly high, up to 2.4V. I'm looking for any suggestions as to what…
I was looking at the EVM design and noticed that on the output grounds and both voltage outputs there is a split in the copper pour going to the headers (J4-J7). I haven't seen that done before and wondered why the board was designed like this.
Part Number: TPS62410 Other Parts Discussed in Thread: TPS62420 , TMS320F28377D , TPS62421 , TPS628511 Hello,
Our existing designs use TPS62420 to provide 1.2V and 3.3V to a TMS320F28377D MCU, plus other devices on the 3.3V rail. But it looks like stock…
Part Number: TPS62420 Other Parts Discussed in Thread: TPS62421 Hello!
I am a little confused when going through the TPS62420 datasheet and looking at the ability to use easyscale.
Section 8.3.5 DEF_1 Pin Functions - makes it seem that EasyScale…
Thanks for the input regarding DC/DC being the way to go.
I ferreted out a buck that would output 1.8V X 2, the TPS62421, and have replaced the LDO in my BOM with the TPS62421 and it's inductors and capacitors. The effect on the price was an extra buck…
Other Parts Discussed in Thread: TPS62420 , TPS62421 , CC3200 , TPS62080 , TPS62085 Require 1.85V for CC3200 in pre-regulated mode. Line and load regulation with less than 2% ripple, 500 mA step current and settling time of < 4 μs with the load step.…