Part Number: IWRL6432 Other Parts Discussed in Thread: TPS628502 , , TPS62442 Would the new TPS62442 dual 2A switcher be a better solution for powering the IWRL6432 radar chip? The TPS62442 has two switchers operating 180 degrees out of phase and would…
Part Number: TPS62442
Can the mode pin on the TPS62442 be changed on the fly? I want to use this part in a radar application. I need the lowest ripple during the active radar chirp, so FPWM mode. But I need light load efficiency during the idle period…
Part Number: TPS62442 Hi team!
I want to use TPS62442 to supply 3A and 1A with each output. What's the difference between these two channels? Can each output supply 3A current? Or can I think that both of the channels are the same?
Part Number: TPS62442-Q1 Hi team,
Customer would like have a TPS62442-Q1 design and simulation with 1A+3A output.
In webech, the current limit in power design page is 0.01A~2A.
Questions:
1. Can you check if some issue in Webech tool?
2. if Webech does…
Part Number: TPS62442-Q1 This is mainly a question out of interest - why do all of our Wide-VIN bucks require a boostrap capacitor and have a max duty cycle of something like 96-98% but then when I look at low-vin devices like TPS62442-Q1, TPS62850x-Q1…
Part Number: TPS62442-Q1 Hello,
I assume yes, but I prefer to check: can TPS62442-Q1 (2A/2A) outputs be multiphased? any caveats there?
Customer application is to power a LTE-Cat 1 NAD, with maximum 3.5A load.
Best regards, Antoine
Part Number: TPS62442-Q1 Other Parts Discussed in Thread: PSPICE-FOR-TI Hello Team,
My customer would like to know if we do have the SPICE model for the device TPS62442-Q1 .
Thanks in advance.
Regards Renan
Part Number: LM26420 Other Parts Discussed in Thread: TPS62442 , TPS62865
Dear team,
1. As mentioned title, Can I combine 2 output for large current up to 4A?
Currently the customer are using LM26420 3 points for their system. but in case of 3.3V, they…