Part Number: TPS62736 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Team,
Please provide a password for the unencrypted SPICE Model for TPS62736.
Thanks
Viktorija
Hello,
- Yes, also attached to the battery is a TPS62736 set to 2.5v and a LTC3221EDC-5 pushing 5v.
- I can't disconnect the 3v rail
- The input to the TPS, the output of the charger (MCP73831T-2ACI/OT), and the battery are directly connected. Bellow…
Part Number: TPS62736 Dear TI support team,
Could you please provide me the raw data of the efficiency curves of the TPS62736 dc/dc converter (Fig. 1 to 6)? I need the data for my Ph.D. As format, Excel or csv files would be perfect!
My addres is jan…
Part Number: TPS62736 When customer download program or debug in PCB, the downloader will bring a 3.3V voltage to the power rail. So Vout will be connect to 3.3V. If Vout will be connected for several hours, it's ok?
Under normal working conditions,…
Part Number: TPS62736 Hi Champs,
do we specify the reverse current which is flowing through the device when the SW/out node is at 3V and the input is 0V?
Other Parts Discussed in Thread: TPS62736 , TPS62740 Does the TPS62736 have protection against running at max rated current or a short for extended period of time? I don't see where this is called out in the specification.
Thanks,
John K.
Other Parts Discussed in Thread: TPS62736 Hi,
in my application I use TPS62736 powered directly by li-ion battery. The TPS62736 circuit is like this: Cin = 4.7 uF + 100 nF, L = 10 uH, Cout = 22 uF, EN1 = GND, EN2 = VIN, voltage divider uses 500 - 900 kOhm…
Other Parts Discussed in Thread: TPS62736 , TPS62743 , TPS63031 , TPS82740A , TPS63051 , TPS61291 Hi,
I want to use TPS62736, TPS62743 Buck and TPS63031 Buck-Boost converters in my designs. But i have some concern:
I need regulated voltages for my CPLD that…
Other Parts Discussed in Thread: TPS62736 I'm using a tps62736 and I want to use the VIN_OK to tell the MCU that the battery need to be charged or not. I'm using a LiPo (4.2v to 3.5v) and a Vout of 3V. The maximum high inout voltage on the MCU is Vdd+0…