Part Number: TPS62802 Other Parts Discussed in Thread: TPS62824A , TPS628301 I am using the TPS62802 to output 1.8V. I have a 10K Pull down at the VSEL/MODE Pin.
I want to run this IC in PWM mode only, however, I do not have a GPIO free on my controller…
Part Number: TPS62802 My customer had procured these two devices TPS62802YKAR and TPS628610YCHR from Digikey.
The top marking on the device is bit different and seen as below with remarks.
Could you please clarify why this disparity?
S.NO
Part n…
Part Number: TPS62802 My TPS62802 generates +3.3VDC output from a USB +5VDC input. I would like to have the DC/DC converter shut down once its input drops below a certain voltage (let's say ~ +4V), to avoid unexpected operation. Currently, regulation…
Part Number: TPS62802 the Above part in inductor new part creation it asking mm2 value for foot print but mentioned diamentions are (x,Y) how to conver that x,y value mm into foot print value mm2..
Part Number: TPS62802 Hi Team,
The input voltage is 3.5V-4.4V, the output voltage is 1.8V. The output cap is 20uF. If using 1uH inductor, will it cause the IC work abnormally?
Best Regards,
Gust
Part Number: TPS62802 Hello,
My customer is using TPS62802 and have a question for R_VSEL resistance value.
They need to configure Vout=3.3V.
Table 1. on the datasheet (SLVSDD1E) says “249.0 or larger” for VSEL=16(3.3V).
On the other hand…
Part Number: TPS62802 Hello
I Designed using TPS62802 under the following conditions
VIN : 3.1V ~ 3.2V
Vour : 3.0V
However, it does not work in PFM mode under Light Load.
So when Vin was increased to 3.7V, PFM worked.
what Is there an input voltage…
Part Number: TPS62802 Dear Sir,
Here is our schematic.
* Test condition
-. Vin = 3.1V
-. Vout = 3.0V
-. Power save mode
1. Issue
-. Quiescent current at power save mode is about 3mA on our b'd.
But, this spec. is 2.5uA on the data sheet…
Part Number: TPS62802 Other Parts Discussed in Thread: TPS62808 Dear,
We saw the TPS62802 datasheet, about PWM Mode IQ current need 8mA?
our application is wireless mouse, but look like not suitable for 2xAA Battery Powered Applications
also we simulation…