Part Number: TPS62871-Q1 Tool/software: Hi support team,
I want to output 0.83V with the TPS62871Y1QWRXSRQ1. I think I'll need to set it via I2C. In that case, does VSEL need to be set to "Short to GND"? Is I2C setting possible when it's set to "47kΩ…
Part Number: TPS62871-Q1 Other Parts Discussed in Thread: TPS62871 Tool/software: Hi team,
My customer Valeo are using TPS62871-Q1 for their project.
For the TPS62871 power (SCH_01) , there are two grounding methods for the compensation loop part…
Part Number: TPS62871-Q1 Tool/software: Hello Team,
I am using this as single device operation, and trying to measure the loop stability. The Vout is given as feedback to VOSNS. Is this the point to inject the noise? Please refer to image below.
Part Number: TPS62871-Q1 Hi Experts,
Is it possible to read or write continuous register values when communicating with the chip in I2C?
For example, I was wondering if I could communicate as shown in the picture below and read 3 bytes with consecutive…
Part Number: TPS62871-Q1 Hello,
My customer is considering using the TPS62871-Q1. They want to use the I2C-less TPS62871-Q1 below, but these devices aren't out yet.
Can they use the devices with I2C connection on TI.com without connecting the…
Part Number: TPS62871-Q1 Hi Team,
For the Tulip family I can see that there is a possibility to read thermal warning for a set of different temperatures
I was wondering if this is done by an integrated temperature sensor and if so, is it possible…
Part Number: TPS62871-Q1 Hello Ti team,
in my design, i use two TPS62871-Q1 in stacked mode to achieve max 18A current . my question is does the two power rails draw the same current(or nearly the same current ) at -40~85℃?
i'm afraid one draw more…