Part Number: TPS62933 Tool/software: Hello
can I use the TPS62933 to input 5V and output -18V . If yes what is may output current value we can reach?
If no is there any apllication to generate -18V using a voltage range 5 to 18V ?
You will find…
Part Number: TPS62933 Tool/software: Hey team,
Customer is looking to dual source the TPS62933 and TPS62933P in the DRLR package. With the only difference being the PG / SS pin changing function, if the capacitor required for SS is left on the PG pin…
Part Number: TPS62933 Other Parts Discussed in Thread: TPS563300 Tool/software: Hello,
I have two TPS62933PDRLR regulators on my PCB to generate 3.3V and 5V from a 12V input.
The schematic and layout for both regulators are quite similar. The 5V regulator…
Part Number: TPS62933 Tool/software: What is the purpose of JP1 in the reference circuit for the TPS62933? Is it necessary for normal operation? If I remove JP1 , will there be any functional or operational issues?
Part Number: TPS62933 Tool/software: Hello TI support,
We intend to make -2.5V/1A inverting output from 6V to 10V input. I gone through some of TI appnotes for designing negative supplies. However, Webench doesn't seems to be supporting latest devices…
Part Number: TPS62933
Tool/software:
Hello, TI members.
Happy new year.
I am using TPS62933 for small servo motor. (5V, 3A motor)
And I have some questions about current and output capacitor. Need some teaching for Power novice.
.
1. What…
Part Number: TPS62933 Tool/software: Hello, is there an easier way to connect the EN pin? Is it possible to set the pin to a fixed voltage or GND? Or does the switching regulator not start? regards
Part Number: TPS62933 Tool/software: Hello,
I am going to use TPS62933 for my system, and I have a qustion about EN pin.
In the datasheet, I can make EN Pin float to turn on device without external control.
I wonder how much time it will take…
Part Number: TPS62933 Tool/software: HI ti team
I am checking the data sheet of TPS62933 and I see that the hot shutdown temperature of TPS62033 is 165 ℃, but its highest junction temperature is 150 ℃. If the temperature of the component exceeds the…