Part Number: TPS63061 We experience a high (almost 100%) failure of TPS63061 in one of our designs. The chip fails when it is repeatedly connected/disconnected to a 12 V power supply.
Part Number: TPS63061 We have been using this DC-DC converter in the design of our signal processing unit. However, our signal acquisition circuit is experiencing significant EMI/noise from the converter, potentially from the switching circuit or inductor…
Part Number: TPS63061 Tool/software: Hello,
I am starting a design with the chip TPS63061DSC.
In the datasheet it suggests to place a inductor (L1) reference Coilcraft XFL4020-102.
This inductor has polarity, but it is not stated anywhere in the…
Part Number: TPS63061 Tool/software: I have configured the TPS63061 according to the TPS6306x datasheet, using guidelines for a fixed voltage version, shown below. Vregin is either 6V or single cell Li-Ion, and RegEn is a matching enable voltage. Looking…
Part Number: TPS63061 Tool/software: Hello, We are using the TPS63061 to provide 5V output to power some of our circuitry. Our design uses solar power as the input to the TPS63061 when our panels are generating enough voltage to power our design. We have…
Part Number: TPS63061 Other Parts Discussed in Thread: TPS63060 Hi Support Team,
we have a few faults (no output voltage + death) of TPS63061 in the schematic below.
Do you have any reference of failure cause or suggestion to optimize the curcuit…
Part Number: TPS63061 Please tell me the internal resistance value (design value) of the FB terminal of TPS63061.
Please refer to the attached document for the location of the resistance.
Part Number: TPS63061 Other Parts Discussed in Thread: TPS63060 , TPS63070 , , TPS62143 Hi!
I used TPS63061 in my board to give 5V fixed output. Input is from a Li-ion battery rated at 11.1V. At lab, I test using a DC adapter with output 13.3V.
…