Part Number: TPS65023-Q1 Other Parts Discussed in Thread: TPS65023
Hello,
We are planning to use TPS65023QRHARQ1 PMIC to power-up the system with nxp's IMX6ULL processor and our system.
Input supply VIN = 5V.
Schematic diagram is attached below.
…
Part Number: TPS65023 Hi Team,
Our customer would like to request the following electrical characteristics of TPS65023QRSBRQ1.
1.ICONST, Internal charge / discharge current on pin TRESPWRON 2.TRESPWRON_LOWTH, Internal lower comparator threshold on pin…
Hello Emily,
Sorry for waiting as I've just received feedback from client as follows:
For your information.
Thank you for your support.
Regards, Archie A.
Part Number: TPS65023 Hi team,
My customer is searching for a power supply solution for Xilinx XCZU4CG. I checked Webench and it recommends TPS65023. But I just want to double check if TPS65023 is suitable for XCZU4CG? And do we have any reference design…
Part Number: TPS65023 Other Parts Discussed in Thread: TPS650250
Hi,
we use all 3 DCDC Converters on the TPS65023 as follows:
Supply Voltage = 5V
------------------------------
DCDC1 = Should be 1.2V but is 2.0V
DCDC2 = 1.8V
DCDC3 = 3.3V
We're using…
Part Number: TPS65023 Other Parts Discussed in Thread: TMS320C6748 , TMS320C6742 , OMAP-L138 Hello guys,
One of my customers is considering using TPS65023 as a power supply for TMS320C6748.
They found the follwowing application note which was written to…
Part Number: TPS65023 Hi TI,
I am supplying 3.3V into TPS65023.
If I want to set VDCDC1 as +1.5V, can it be done using external resistor divider on DEFDCDC1? Or must it be set using DEFCORE register via I2C interface?
thanks.
Part Number: TPS65023-Q1 Other Parts Discussed in Thread: TPS65023 , LM26480 Hi,
I was not able to find any PSRR data for the internal LDOs of the TPS65023.
Do you by chance have any data?
Thanks
Regards,
Alberto
Part Number: TPS65023-Q1 Other Parts Discussed in Thread: TPS65023 , TPS56C215 , TIDA-01480 , TPS62067 , , TPS568215 Hi Team,
Would you advise TI best match power solution for XAZU5EV FPGA?
I found TPS65023 is recommended for ZU5EV.
However I'm not sure…