Part Number: TPS65140-Q1 Hi Sir,
My customer is looking for a replacement device for RTQ6749-QT-A2, could you please advise if there have any solutions?
RTQ6749-QT-A2:
DSQ6749-QT-A2-02.pdf
Part Number: TPS65140-Q1 Other Parts Discussed in Thread: TPS65140 , TPS65131 Hi team,
My customer only uses the negative and positive charge pump and LDO for +18V and -11V. They don't need the boost converter output. But I see the SUP pin need to be connected…
Part Number: TPS65140-Q1 Other Parts Discussed in Thread: PMP9780 , TPS65131 Dear team,
Could you please help recommend one appropriate device to support below LCD specs? VIN=VDD=3.3V, there are four output voltages as below.
Thanks & Best Regards,…
Part Number: TPS65140-Q1 Other Parts Discussed in Thread: TPS65140 , TPS65141 Hi, I am Hwadong Song of TOVIS
As I wroted in title, our tps65140 power circuit doesn't work well.
Specifically, the output is too low(0V or 7V). So could you check wheth…
Other Parts Discussed in Thread: TPS65140 0083.TPS65140-Q1 Vo3 drop .ppt
When I had 2mA from no load, the output of Vo3 falls approximately 0.5V.
Why is it? Please watch an attached file.
Will it be necessary to confirm phase margin of Vo2, Vo3 and Vo4?
In the case of Yes.
Please tell me how I should measure phase margin of Vo2, Vo3 and Vo4.
When I cannot measure it, please tell me the reason.
Hello Nate,
What do you mean with "the target voltage is not fixed"?
I think TPS65140-Q1 should be a good fit for replacing MAX16928. Did you find the time to check the components Diaara recommended? I think TPS65131-Q1 does not fit as good…
Part Number: TPS65100-Q1 Other Parts Discussed in Thread: TPS65140-Q1 , TPS65150-Q1 Customer is reviewing TPS65100-Q1 on LCD panel for their connected audio project. Below is their start-up sequence requirement. Can TPS65100-Q1 support this timing requirement…