Part Number: TPS65185 Hello
We have based our design on the TPS65185EVM. The TPS consumes high current if switched on. (about 500mA)
In our PCB is the winding start of the inductors L1, L2 is swapped compared to the reference design. Does the inverted position…
Part Number: TPS65185 Hello,
The TPS65185 requires an external 10k NTC for temperature measurment. I have no information about exact parameters of the NTC, especially the Beta coefficient, that seems important for me to get a good temperature measurment…
Hi Jacky,
I don't think there is a requirement on VF, the main impact of VF should be efficiency. Smaller Vf values have better efficiency than larger ones.
Current rating is important. All of the diodes used for validation of this part were rated…
Pedro Rodrigues6 said:
... The way I found to unbrick my device was to...
I can confirm that the procedure described above works on an freshly shipped, unbricked unit. I.e.
Update the USB-GPIO adapter firmware with the BQ2416x EVM's software: This…
Hi Yusuke-san,
I'm not sure I understand their concern, could you elaborate on their conditions?
Also, the EVM is available on the website so they could test out their conditions on the actual IC, would they be willing to evaluate the device?
…
Janice,
Thank you for reply. We expect to new GUI for PMIC. We want to know about method of operation for register to the TPS65185 at using HPA172.
Currently, our customer has a HPA172 and a TPS65185EVM. They do not able to use those. We want to resolve…
Part Number: USB-TO-GPIO Hi,
I have USB-TO-GPIO from TPS65185 kit . At first, when I plugged it into USB, everything was fine, but then I ran TPS65185 GUI and it asked me to update firmware. Since then LED did not light up and interface is recognised…