Part Number: TPS65218EVM-100 Other Parts Discussed in Thread: USB2ANY , IPG-UI , TIDA-00606 Hi,
We are facing communication issue with IPGUI to TPS65218EVM-100, So as we turn ON EVM kit with input VSYS (5V/3A) we are getting the default outputs which mentioned…
Part Number: TPS65218EVM-100 Other Parts Discussed in Thread: USB2ANY , , IPG-UI Hi,
I am having trouble using the IPG-UI with the TPS65218EVM-100 + USB2ANY.
As you can see below the register I am reading are wrong, It seems to be reading random values…
Part Number: TPS65218EVM-100 Other Parts Discussed in Thread: TPS65218 , USB2ANY , IPG-UI I have one TPS65218EVM, USB2ANY and i installed the TPS65218 GUI software from the below link. I have connected and give 5V, 3V power as said in datasheet.I am not…
Part Number: TPS65218EVM-100 Other Parts Discussed in Thread: IPG-UI Hello all,
I'm using TPS65218EVM and IPG-GUI. I'm going to change output voltage for DCDC1 and 2.
But both DCDCs were not changed. Output voltage for other DCDCs and LDO were…
Hi Satoshi,
I have provided a couple scope captures of the power-up sequence from a TPS65218D0 chip that is used in our TPS65218EVM-100 board. I am seeing ~2ms between DCDC3 and LS1:
Can you show DCDC6, DCDC3, and LS1 in one capture similar to the ones…
Part Number: TPS65218EVM-100 Other Parts Discussed in Thread: USB2ANY , TPS65218 Is the USB2ANY included in the kit for TPS65218EVM-100?
Looking at the User's Guide it indicates the following:
EVM Kit
The EVM kit ( Figure 1 ) contains the following…
Part Number: TPS65218D0 Other Parts Discussed in Thread: TPS65218 , TPS6521815 , IPG-UI , TMUX7413F , TPS65218EVM-100 , BOOSTXL-TPS65218 Hi All,
I have a question about TPS65218D0.
I want the power sequence to be in the following order DCDC1 -> DCDC2 -> DCDC3…
Part Number: TPS6521855 Other Parts Discussed in Thread: TPS65218 , , TPS65218EVM-100 Hi team,
Do you have any data on start up time for DCDC, LDO, and LS?
The customer is concerned if they are going to rise too quickly without soft start.
Best Regards…
Hi Brenda,
Thanks for the VERY fast feedback!
2 more questions:
1) I'm using the eval board TPS65218EVM-100 and not the BoosterPack, should I understand that the file you indicated is working for this eval board too?
2) I tried the link all day long…
Hi Kengo,
I can't guarantee the consequences of having those output pins connected to GND because we do not validate connections that are not recommended.
However, this device has an EVM ( TPS65218EVM-100 ) for our customers to evaluate the PMIC features…