Part Number: TPS65233-1 Table 6.3 Recommended Operating Conditions specs the Junction Temperature range from -40 to 85 C, but calls it Ta. Does the table mean Ta (ambient temperature) or Tj (junction temperature?
Part Number: TPS65233-1 We operate the device in non I2C mode
We would like to control the 22Khz generation using the EXTM pin as described in paragraph 7.4.1 of the data sheet - option 2
When toggling EXTM in 22khz we get the 22Khz output - option 1 …
Part Number: TPS65233-1 Good day Colleagues,
Could you tell me if it's possible to set the current limit below 350mA?
Customer wants to set it around 250mA. Are there any limitations of the lowest levels?
Thank you, Mike
Part Number: TPS65233-1 Other Parts Discussed in Thread: TPS65233 Hi Sir
If new project use TPS65233-1 ,may I use 22uH (TPS65233 reference design use) for TPS65233-1 ?
or I need to follow 10uH~4.7uH in datasheet ?
Thanks
Part Number: TPS65233-1 Other Parts Discussed in Thread: TPS65233 Dear Team,
Can you please advise on the customer question below ?
I would like to use it with I2C slave address = 0x61.
According to the DS , the addr pin is muxed with the EN pin.
For…
Part Number: TPS65233-1 Other Parts Discussed in Thread: TPS65233 , Dear Sir
1. May I know what's different between TPS65233 andd TPS65233-1 ?
2. We need to support Vin=15.6V (12V*130%) ,may I know TPS65233-1 could support Vout = 13V/18V and iout typ…
Part Number: TPS65233-1 HI Sir
I saw TI have two recommend surge protection circuit ,May I know below two circuit can support 2KV surge ?
So far we test 1.75KV surge ,VLNB pin of TPS65233-1 will damage
Thanks
Part Number: TPS65233-1 Other Parts Discussed in Thread: TPS65235-1 , TPS65235 HI SIr
We are using TPS65233-1 have audible noise
1. Do you have any experience of this issue ? how to solve
2. I saw TPS65235-1 have avoid audible function ,may i know the…
Part Number: TPS65233-1 Other Parts Discussed in Thread: TPS65233EVM , TPS65233 , TPS65235-1
Hi,
I'm looking at the datasheet and find 3 diodes in the reference schematic. The very same reference found in the evaluation board TPS65233EVM". However in…
Part Number: TPS65235 Other Parts Discussed in Thread: TPS65233 Dear SIr
May I know
1. TPS65235-1 have a better price than TPS65233 ,if the R/R is the same
2. How about the TPS65235-1 surge test result ?? if we need pass surge +/- 4KV ,does TI have any…