Part Number: TPS65235-1 Other Parts Discussed in Thread: TPS65235 , TPS652353 Tool/software: We are using a TPS65235-1 with Rset of 330k. This means that our current limit should be at 440mA.
However, we are finding that the current limits at about…
Part Number: TPS65235-1 Other Parts Discussed in Thread: USB-TO-GPIO2 Tool/software: Wanting confirmation on if the TPS65235-1EVM-747 comes with a USB-TO-GPIO because UG says 'The EVM kit includes the USB-TO-GPIO interface box' But it also says 'The EVM…
Part Number: TPS65235
Hi
May I know the main difference between TPS65235 and TPS65235-1? By comparing the both datasheets, it seems like the only difference is the support of FCCM.
I have two questions:
If we are not using FCCM mode, then TPS65235…
Part Number: TPS65235-1
Hello,
Our customer has a question if TPS65235-1 has a potential issue in his application.
In his application, 12.7V boost input voltage is dropped to 12.4V for 10ms then back to 12.7V, while it works 19V VLNB. Even though…
Part Number: TPS65235-1 Other Parts Discussed in Thread: TPS652353 , Hello,
Our customer asked about how TPS65235-1, TPS652353 respond if he accesses unassigned I2C register like 0x03. Do TPS65235-1, TPS652353 respond anything like ACK for example.…
Part Number: TPS65235-1 Dear,
I need your advice to help me understand of TPS65235-1 Vin correctly.
According to data sheets, it has the range of 4.5V - 20V , but it is different in the comparison table on the website, it which it is 4.5V - 16V .…
Part Number: TPS65235-1 Other Parts Discussed in Thread: TPS65235 Hi,
Could you please tell me DiSEqC protocol ?
Q1. Can TPS65235-1 convert I2C data to 22kHz tone signal and convert 22kHz tone signal to I2C data if transmitting and receiving with…
Part Number: TPS65235-1 Hi,
Could you please tell me whether TPS65235-1 can be used as only use tone detection ? If possible, I am considering reducing BOM cost as TPS65235-1 isn't used as the boost converter. So, could you please give me your advice…
Part Number: TPS65235-1 Hi,
Could you please tell me whether EN pin can be pulled up to 3.3V or 5V with the pull-up resistor in order to using TPS65235-1 without controlling EN pin via GPIO ?
Best regards, Kato
Part Number: TPS65235-1 Other Parts Discussed in Thread: TPS65233 Hi, Team,
Absolute Min spec of VIN, LX, BOOST, VLNB are 1. Is this description error?
Best Regards, Satoshi Yone