Part Number: TPS65235-1 Hi, Team,
For D/S Table 3, are there EN/SCL/VCTRL pin configuration recommendation when I2C_CON = 1?
Best Regards, Satoshi Yone
Part Number: TPS65235-1 Hello,
Our customer asked about how OCP status bit sets after Hiccup timer is expired. Does it keep 1b state until processor read OCP register or set 0b state as soon as the hiccup timer is expired.
Best regards,
Part Number: TPS65235-1 Dear,
I need your advice to help me understand of TPS65235-1 Vin correctly.
According to data sheets, it has the range of 4.5V - 20V , but it is different in the comparison table on the website, it which it is 4.5V - 16V .
The Website…
Other Parts Discussed in Thread: TPS65235-1 Dear,
I have a simple question for TPS65235-1 Vin Power Rail, which is supposed to be 5V, 12V and 15V. I've understood that most LNB receiver is working in 12V Vin power platform.
Here my question is if there…
Part Number: TPS65235-1 dear all,
I have a new request from my customer on tps65235-1 as follows:
bit#4 (field T125) =0 all the times which means by datasheet that Die temp is above 125degC (Even at cold start up).
Customer checked temp of the device on…
Zixu,
thank you for detailed answer.
However, The solution in TPS65235 AN is a different IC TPS65235-1, which canceled internal OVP comparator so the ripple frequency changed. How can I apply the fix in my case?
/Roland
Part Number: TPS65235-1 Hi Team,
We understand that the recommended minimum actual capacity of Boost Capacitance is 5uF at 10uH.
Is my understanding correct?
If no, could you please let us know the recommended value?
Regards,
Kanemaru
Part Number: TPS65235-1 Hi Team,
Our customer would like to know the L2 of function on TPS65235-1EVM-694.
So, why is this inductor necessary?
And, does an evil not occur even if this inductor isn’t placed?
Could you please let us know if you have…
Part Number: TPS65235 Dear Sir
We saw diodes solution ZLPM8014 can support 21Vout for DiSEqC2.0 application
Could TPS65235-1 support 21Vout or TI have another solution can support ?
Thanks
Part Number: TPS65235 Other Parts Discussed in Thread: TPS65233 Dear SIr
May I know
1. TPS65235-1 have a better price than TPS65233 ,if the R/R is the same
2. How about the TPS65235-1 surge test result ?? if we need pass surge +/- 4KV ,does TI have any…