Part Number: TPS652353 Dear All
Is possible to use the DIN and DOUT (demodulation of external 22KHz tone) when Vlnb out is disable ?
If I set BIT3 in CR2, on pin DIN I have around 2.5V and the 22Khz tone from external source (a receiiver, i.e.)
If I clear…
Part Number: TPS652353 Other Parts Discussed in Thread: TPS65235-1 Hi team,
The customer used TPS652353 setting ISET to 110kohm for 1A current limit. And hiccup ON time set to 58 ms and OFF time set to 466 ms.
But they found the abnormal protection function…
Part Number: TPS652353
Hi,
I am using TPS652353 in my design and using I2C to control it.
It works fine for setting voltage levels, I am using 13.4V and 18.2V which work fine.
But. when I try to disable the output by writing 0x00 in Control 2 register…
Part Number: TPS652353 Hi,
i need just a small clarification.
TPS652353 LNB regulator IC supports maximum current output of 1A.
Is there a standard which tells LNBs to limit the current requirement within this limit?
Part Number: TPS652353
Hi,
I had earlier requested a design review here for my TPS652353 design.
Now my board has arrived and I wanted to check the output voltage by setting it through I2C.
My input voltage is 5 Volts, I have connected VCC and VIN pins…
Part Number: TPS652353 Hi,
Pleas review this schematic for me. My input voltage is 15V coming from a Power module outside the PCB. The control logic is TTL 5V. I will either use I2C or combination of TTL logic according to datasheet truth table to set…
Part Number: TPS652353 Other Parts Discussed in Thread: TPS65235-1 Hello,
Our customer has asked us if TPS652353 and TPS65235-1 have a device ID register to identify either one is mounted. Although I have not seen such a device ID kind of register in…
Part Number: TPS652353 Other Parts Discussed in Thread: TPS65235-1 Hello,
Our customer asked about OCP Hiccup timer definition differences between TPS65235-1 and TPS65235-3.
When he checked the differences between two device in the datasheet, he had a…
Part Number: TPS65235-1EVM-694 hello,
Our customer has asked if TPS65235-1EVM-694 GUI is absolutely same as that of TPS652353 EVM even we know the difference is OCP Hiccup timer setting.
Could you help him out if these GUI software is absolutely same…