Part Number: TPS65251-3 Tool/software: Hi team,
Could you clarify the slope rate of the load change in datasheet?
TPS65251-x 4.5-V to 18-V Input, High Current, Synchronous Step Down datasheet (Rev. B) (ti.com)
Part Number: TPS65251 Hi Team,
Could you show the difference between TPS65251 and TPS65251-x, as well as difference between TPS65251-1, TPS65251-2 and TPS65251-3?
I looked at the datasheet but didn't find...
thanks a lot.
Best regards,
…
Part Number: TPS65251 Hi, Team
My communication customer is using TPS65251-3 in their small cell products. They find the output voltage will drop during startup, if the outpu voltage is set to > 3.5V.
Here is customer schematic. The CH3 of TPS65251…
Other Parts Discussed in Thread: TPS65251-3 , TPS65251-2 , TPS65251-Q1 , TPS65251-1 , TPS65251 Hello,
Please advice how to process following terminals when I do not use back2.
LX2
VIN2
BST2
EN2
RLIM2
SS2
CMP2
FB2
Best Regards…
Hi, Jordan
I review your schematic, it is okay, but layout is bad.
I think the issue is caused by bad layout, suggest place 30ea VIAs at thermal pad.
I attached a layout guideline for your reference.
TPS6525x_LAYOUT_GUIDE.ppt
Part Number: TPS65251 Hi Team,
The new design of a motherboard scheme, in which the power part uses the circuit of TPS65251 which has been verified before, but when the board comes back, TPS65251 has no output, the old and new schematic diagram is as…
Part Number: TPS65251 Hi I'm using the TPS65251 to create 3 voltage rails and have a design very similar to the reference design in the datasheet and the reference device.
When powering on the board with no load I was getting the correct voltages on…
Part Number: TPS652510 Other Parts Discussed in Thread: TPS65263 , TPS65261 , TPS65251 Dear TI,
I'm going to use this part TPS652510 with 3 rail power in XC7A35T FBGA:
- 1V / 2A for VCORE
- 1.8V / 2A for VAUX
- 3.3V / 3A for VCCIO
Since WeBench…