Part Number: TPS65261-1 Hi team
My customer requested to review compensation value of TPS65261-1.
I had schematic of customer.
But I don't share E2E community, because it is confidential issue.
If you tell me how to connect with you, I will send you…
Part Number: TPS65261-1 Hi,
We got a question from customer about TPS65261-1
Could you help us?
[Question]
Can the output voltage be set from the feedback voltage 0.6 V ?
Is it possible to output less than 1.0 V ?
Thank you
Best regards
Part Number: TPS65261 Hi team,
The datasheet describes TPS65261 and TPS65261-1 has OVP. I want to know how much time it takes from over voltage detection to protection.
Regards, Saito
Part Number: TPS65261 Hi, I have the same issue however I am using MODE, EN1,EN2 and EN3 for sequenced start up.
I have MODE, EN1 and EN2 connected to V7V and EN3 connected to the Power good of another supply.
The intention was to use V7V to power the…
Part Number: TPS65261-1 Other Parts Discussed in Thread: TPS65261
Tool/software: WEBENCH® Design Tools
Hi team.
I did simulation for TPS65261-1 via WEBENCH.
However, the bode plot result of Vout3 was output in a different form than normal.
It is…
Other Parts Discussed in Thread: TPS65261 I have questions about TPS65261.
Please check the attached document.
We want to set sequence.
1.1V→1.5V→2.5V→1.8V→3.3V
PG of TPS65261① connects to EN3 pin of TPS65261②.
Question 1.
Are there…
Part Number: TPS65261-1 Hello Non-Isolated DC/DC Experts,
Do we have temperature cycling data for the TPS65261-1? Mechanical stress due to temperature cycling?
Part Number: TPS65261 Hi,
I am bringing up a board and have not been able to get the TPS65261 powered up. One issue I notice is that the V7V pin never outputs any voltage above ~10 mV. From the datasheet, it seems like V7V should track the input voltage…