Part Number: TPS65262-2 Hi,
I am using TPS65262-2RHBT in my design. I have to the control the power sequence externally and maintain certain sequence. Please let me know how can I control the sequence externally. Also I have to control the sequence of…
Part Number: TPS653852A-Q1 Other Parts Discussed in Thread: TPS65262 , TPS65811 Hi Team,
There is a good new that we could DIN TI product!
Do we have a solution that could me following spec? THX
PMIC Spec.
1
Vin
4V~30V(Maximum input voltage…
Part Number: TPS65262-2 Dear Team,
Hello, I would like to inquire about the protection operation of TP65262-2.
(1). Is it correct to operate in Hic-cup mode when the TP65262-2 IC chip has over current protection and short circuit?
(2). When the output…
Part Number: TPS65262-2 Hi TI Team,
We are planning to use TPS65262-2 for generating on-board supplies for different interfaces on our board from 5V input. The requirement and our plan is as below
Buck 1 for 3.3V, 3A supply
Buck 2 for 2.5V, 1A supply …
Hi, James
I afraid there is no such devices including 1 buck + 2 LDOs.
TPS65262 has 3 bucks + 2 LDOs, if no use 2 bucks, you can pull EN2=EN3=low and floating other pins.
Part Number: TPS65262-2 Hello Our customer is applying TPS65262-2RHBR. The applicable specifications are as follows. VIN = 5 V Voutput = Buck 1 / 3.3V, Buck 2 / 3.3V, Buck 3 / 1.5V problem
1. Buck2 is Enable, but PWM output is 0V.
2. Buck3 is Enable, but 2…
Part Number: TPS65262-2 Hello, customer will use TPS65262-2 powering the Altera FPGA. it requires voltage accuracy from ext. DC/DC power shall be within +/-2.7% for 1.1V rail.
How to calculate the output voltage accuracy of the TPS65262-2 with 1% tolerance…
Part Number: TPS54260 Other Parts Discussed in Thread: TPS64200 , TPS40000 , TPS40040 , TPS40021-EP , TPS40007 , TPS65262-1 , TPS53353 , TPS53513 , TPS53355 , TPS53515 , TPS53318 , TPS53319 , TPS53915 I am anxious to use the concepts presented in TI’s PMP5863 Reference…
Other Parts Discussed in Thread: TPS65262 , TPS65262-1 Hello
My Customer is interested in TPS65262, and TPS65262-1 .
Would you please let me know the Current protection type such as Fold Back/ Reset/ Latch-Off ?
Best Regards