Part Number: TPS65265 Tool/software: WEBENCH® Design Tools I understand the current TI WEBENCH tool doesn't support PMU devices like TPS65265 now.
Is there any other way we still can use WEBENCH tool to help our design with TPS65265? Can we select a…
Part Number: TPS65265 Other Parts Discussed in Thread: UCD9081 , Hi,
1. If I use UCD9081 for sequence the TPS65265 ENx, can I floating SEQ_DLY, PG_DLY, PGOOD pins?
2. If the PSM Mode is beater than PWM Mode why did you leave the option to choose between them…
Part Number: TPS65265 Hi Team,
My customer is using TPS65265 and has some concerns about the enable function.
1. TPS65265 can start up normally with EN pin open or external 5V signal.
2. TPS65265 cannot start up by customer's external transistor control…
Part Number: TPS65265 I have some simple questions about TPS65265. This is 3 output Buck Regulator.
I want to control EN1/EN2/EN3 seperatly.
From the datesheet, If i make Mode Pin(#7) floating then, Buck1/2/3 are controlled separate by EN1/2/3.
And in…
Part Number: TPS65265 Tool/software: WEBENCH® Design Tools Hi,
I had been trying to retrieve the TPS65265RHBR PMU design from my WEBENCH design page, but all the designs that related to TPS65265RHBR had become red and unable to open. I was wondering if…
Part Number: TPS65265 Hi,
I have using this regulator for Intel Platforms for the output (2.6V, 0.65A),(1.8V, 1.21A),(1.0V, 1.86A). Please help me whether we need Input Filter for this design, If yes is there any reference schematics available, in datasheet…
Part Number: TPS65265 Other Parts Discussed in Thread: TPS65400 Hi,
We are using TPS65265 for triple output needs, I see the IC supports 3 EN pins, which we can use for sequencing, but our requirement also asks us to have 3 separate PowerGOOD pins, is…
Part Number: TPS65265 Hi,
I am testing on a board that uses the TPS65265 to generate several voltages.
One of our supplies generated by the TPS65265, which has a nominal voltage of 1.2V, has a nominal current load of 50mA, but has transient loads of ~400mA…
Part Number: TPS65265
Hi, Team
My communication customer plan to use TPS65265 to convert 12V to 7V, but the maximum output voltage in Webench is only 5.5V.
Could you help to confirm whether TPS65265 can support 12V to 7V conversion?
Thanks
Kevin