Hi Matthew,
Thanks for coming to us with your queries. Please kindly find 3D model in below link.
https://vendor.ultralibrarian.com/TI/embedded/?gpn=TPS65266&package=RHB&pin=32&sid=0178b0799bda0021c00ff59f259403072001b06a007e8&c=1
After…
Part Number: TPS65266 Other Parts Discussed in Thread: LP8758 Hi,
I had used TPS65266RHBR in my previous design of board. But there is slight change in the design and I am looking for a new PMIC with below requirements:
Vin(typical)= 3.3V
Vout 1: 1.1V Iout1…
Hi, Sir
TPS65266 is Forced PWM, it will keep switching.
TPS65266-1 is PSM, switching frequency will skip, as for the PSM operation, you can refer the datasheet of page22.
Could you probe the Vout and LX waveforms at the same time? then to check what…
Part Number: TPS65266
Hi,
I am using TPS65266 in my design. I have attached the schematics. Can someone please review the schematics and let us know your feedbacks on the same.
My requirement is as below.
1488.PMIC.pdf 1. Vin=5V
2. Buck1: Vout=1.8V Iout…
Part Number: TPS65266 Hi,
I am planning to use TPS65266 in my design. My requirement is as below.
Buck1: 1.8V
Buck2: 3.3V
Buck3: 1.15V
Kindly help me in solving below queries:
1. I will be enabling Buck2 first and then Buck1 and Buck3. This should not…
Part Number: TPS65266 Other Parts Discussed in Thread: TPS65261 Hello,
Please clarify my doubts related to TPS65266-1 regulator below:
1. How to control(Enable/Disable) Outputs of the DC-DC regulator: TPS65266-1 ??
2. Is there any possibility of getting…
Hi,
Relative high current at no load current is because TPS65266 works in Force Continuous Conduction Mode(FCCM).
You can refer to related description in datasheet. This mode can maintain small ripple at light load, while the compromise is lower efficiency…
Other Parts Discussed in Thread: TPS65266 , TPS65217 , TPS65218D0 , BQ25898 , BQ25600 Dear sir:
In our designing, we need two IC as below:
1) charging IC: charger current is about 2A and for 4.2V battery.
2) PMU IC: need at least three DC-DC…
Other Parts Discussed in Thread: TPS65266 Hi,
I posted about a month ago about a TPS65266 that wasn't outputting a voltage when supplied with an input voltage and was told to redesign my PCB.
I have done that and added a few components to make my…
Part Number: TPS65266 Hi,
From the datasheet:
min/typ/max
VENXH EN1/2/3 high-level input voltage:-/1.2V/ 1.26V VENXL EN1/2/3 low-level input voltage: 1.1V/ 1.15V/-
Question1 - Does this information means:
- If I want to enable: set 1.2V to 1.26V max?
…