Part Number: TPS65295 Hi,
I'm using the TPS65295 in my design which doesn't need to support the S3 state. In this case, can the SLP_S4 and VTT_CNTL inputs be shorted and controlled be a single driving source to enable/disable the device? Also, the datasheet…
Part Number: TPS65295 Hi,
I am using TPS65295 IC for our DDR4 power solution. I have some queries.
Does bootstrap connection required for SW_VPP(2.5V generation) pin? (In pin description its mentioned “ VPP switching node connection to the inductor…
Part Number: TPS65295 Hi Sir,
may i know is there an efficiency curve for PVIN +5v ? because the datasheet only up to 7.4v.
or have other data about the test results of TPS65295 for PVIN +5V. thanks for your help.
Part Number: TPS65295 Hi team,
my customer has a height restriction (3.5mm MAX) on their board and so they must choose a different inductor than what is recommended in the datsheet.
for the VDDQSNS inductor, they found the Signal Transformer SCIHP0420TB…
Part Number: TPS65295 The footprint shown on page P31 of tps65295 datasheet is rje0018b, but there is rje0018a in the back, but there is only one packaging form vqfn in the ordering information. Which should be followed when making PCB? The two are encapsulated…
Part Number: TPS65295 In the current data sheet, which set of package dimension drawings are we supposed to use? There are two. Also, the dimensions for the locations of pins 7, 8,9, 16, 17,18 are not clear. What are their distances from the package center…
Part Number: TPS65295 Hello Team,
Input is correctly 1.2V. However When evaluating TPS65295, VTT has 0.9V regardless its expected voltage is 0.6V.
In this settings, VTTREF=Open.
When put capacitor on VTTREF, VTT has 0.6V.
Could you let me know appropriate…
Part Number: TPS65295 Hello
I am going to use TPS65295RJER.
Before mounting the components on the board, we are trying to estimate the temperature of Tj from Ta set by Theta Ja described in the data sheet. However, TPS65295RJER has multiple built-in…
Part Number: TPS65295 Hi Sir
May I know which platform that TPS65295 could be used ? due to Whiskey lake need 12A
Below information is from "WHL-U Power Map_Rev1.0.xlsm" Intel document
Part Number: TPS65295 Hi,
This is the first usage of TPS65295 in my customer. comparing to TPS65295EVM-079 schematic, I just can see a few difference on the BOM. please kindly give your professional advice. thanks.
VTT.pdf