Part Number: TPS65320D-Q1 Hi,
1.Please tell me the input voltage and output voltage when you measured the efficiency of Fig. 23.
2.As the measurement circuit is shown in the figure below, I assume that the output voltage is 5V. Is this correct?…
Part Number: TPS65320D-Q1 Other Parts Discussed in Thread: TLV1117LV Tool/software: Will the DC/DC and LDO outputs have stable voltage when the input voltage fluctuates? We know it's normal for the voltage of the car battery to fluctuate several volts…
Part Number: TPS65320D-Q1 Tool/software: I'm attempting to calculate the max switching frequency for my application using equations 4 and 5 from the datasheet (pg. 14).
Question:
Given that equation 5 only applies during a short-circuit event…
Part Number: TPS65320D-Q1 Tool/software: Hi Team,
I notice the package info in TPS65320D-Q1 datasheet is inconsistent.
1st page shows HTSSOP but the bottom shows TSSOP and it also have 2 different package info, one is PWP0014G, the other one is…
Part Number: TPS65320D-Q1 Tool/software: Hi,team
I am considering using the TPS65320D and have a question about EN.
The absolute maximum rating of EN-Vin is 1V.
Is there a possibility of damage if a voltage greater than 1V is applied for even a…
Part Number: TPS65320D-Q1 Hi
We use the TPS65320D-Q1 Buck-Regulator output to transfer 3.3v to the MCU, and the MCU will turn on the LDO enable pin and mosfet to transfer 1.2 and 1.5v. The current problem is When the MCU turns on the MOS and LDO enable…
Part Number: TPS65320D-Q1 Hi, Support Team
We want to know TPS65320D-Q1 operating vaule?
Design input:
Vin=12V
Vout=3.3V
Iout=0.000007A
Fixed frequency PWM control
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrenc…
Part Number: TPS65320D-Q1 Hello team
could you please take a look on my customers question and comment on possibility combining the outputs
From what I understand they want to use the BUCK and the LDO for the same rail and basically turn off the…
Part Number: TPS65320-Q1 Other Parts Discussed in Thread: TPS65320D-Q1 In the current design, TPS65320D-Q1 is used to convert 12V to 3.3V by buck regulator and the LDO is used to convert 3.3v to 1.2V.
1. There is currently an inrush current issue with…
Part Number: TPS65320D-Q1 Hi Exert:
our customer is asking TPS65320DQPWPRQ1 FIT /pin FMEA functional safety report , I found the PMIC is non functional safety PMIC.
do we have other same function PMIC (one Buck + one LDO) which have FIT /pin FMEA…