Part Number: TPS65320D-Q1 Other Parts Discussed in Thread: TPS65320-Q1 Dears
Currently we are using one TI power IC(TPS65320-Q1) in our product, But we are facing a problem in our degin:
This power regulator output 3V3 & 1V8 rail, and there is one power…
Part Number: TPS65320D-Q1 Other Parts Discussed in Thread: TPS43330-Q1 Hello,
When use TPS65320D-Q1 for automotive product (Front camera module)design, We observe the load transient performs do not meet our product, The detail description please refer…
Part Number: TPS65320D-Q1 Hi there,
In the block diagram of TPS65320D-Q1, there is a resistor between Pin GND and Pin PowerPad. My customer is wondering the value of the resistance.
Can you help to answer this?
Thank you!
Pin
Part Number: TPS65320D-Q1 Hai TI support,
I have a question regarding the TI part TPS65320DQPWPRQ1,
According to datasheet as below, the VH min is 2.5V and VL max is 0.7V.
But the actual test results are as below :
Note : - Blue line is EN1 (Buck…
Part Number: TPS65320D-Q1 Hi,
I would like to simulate TPS65320D's small signal model as describe at the datasheet paragraph 7.3.1.17 . For that I have to know the error amplifier parameters Aol and BW . What should be the value of these parameters…
Part Number: TPS65320D-Q1
Hello,
We are using TPS65320D-Q1 in our design.
This email is regarding one enquiry related to NRST pin (Pin6 ) in our TPS65320D-Q1 schematic.
Do we need to mount an external 10K pull resistor for NRST pin (pin 6) connected to…
Part Number: TPS65320D-Q1
I would like to get 12V/2A in the output of the device what should be the minimum Vin ?
What is the maximum leakage current in idle with no load .
Part Number: TPS65320D-Q1 Hi,
I would like to create "dithering" by adjusting the BUCK switching frequency from external source ( MCU) .
Will the BUCK stay stable while changing its switching frequency dynamically ?
What is the minimal time…
Part Number: TPS65320D-Q1 In the data sheet it states:
"7.3.5 Enable and Undervoltage Lockout
The TPS65320D-Q1 device enable pins (EN1 and EN2) are high-voltage-tolerant input pins with an internal pulldown circuit..."
Can you tell us what…