Part Number: TPS65321A-Q1 Other Parts Discussed in Thread: TPS65321-Q1 ,
Hi Team,
My customer would like to figure out the difference between TPS65321A-Q1 and TPS65321-Q1.
Do we have a statement about this difference?
If customer still use TPS65321, do…
Other Parts Discussed in Thread: TPS65321-Q1 Hi, Team
An automotive customer GAC plan to use TPS65321-Q1 in their car infotainment system. Both input of DC/DC and LDO are connected to 12V battery, and both output is 5V.
If the output of LDO is shorted…
Hello,
I want to make sure I understood your request. You want to replace the PMIC TPS65381 by simple LDOs and you need 2 rails 5V or 3.3V and 1.2V. What is the current consumption on each rail?
There is an option single device (TPS65320-Q1 or TPS65321…
Hello, Walter,
in that respect yes, they share the same over-temperature protection, see datasheet section 7.3.1.15 for TPS65320-Q1 and section 7.3.3 for TPS65321-Q1.
Best regards,
Frank
Other Parts Discussed in Thread: TPS65320-Q1 Hi there,
We love the built-in LDO with auto-source so that we can shut down the buck regulator during sleep mode, but 3.2A capability is a bit excessive.
Are there any similar chips more suited to an operating…