Part Number: TPS65400-Q1
Hi,
I'm from the Lidar group in Intel.
PMIC Power esimations.xlsx
We have a real concern regarding the power dissipation of this PMIC.
Our maximum ratings are as following:
- 2 rails of 4A each, 1 rail of 2 A and one rail…
Part Number: TPS65400-Q1 Other Parts Discussed in Thread: TPS54331 , TPS54231 , TPS54335A , TPS560430-Q1 Hi,
AEC Grade 1 means the ambient temperature is -40 to 125°C.
So the operating junction temperature should be above 125°C due to the power dissipation…
Part Number: TPS65400-Q1Tps65400-q1: Is the factory NVM data in the IC I purchased on the official website the same as the NVM data in the PMIC of the Demo development board I purchased?By what means, is it the same?
Part Number: TPS65400-Q1 Other Parts Discussed in Thread: TPS65279 , LM61460 , LM62460-Q1 , TPS7H4010-SEP Hello,
I've been shopping for a while trying to identify the best buck regulators for a design that will have:
14V < Vin < 18V
Vout1 = 12V…
Part Number: TPS65400-Q1 i'm trying to work out the comp loop values using the web based power designer. the tool seems to get stuck on L values (very narrow range), and i don't trust the loop comp values as a result. if i look at the equations…
Part Number: TPS65400-Q1
I have a design in which I use the first three outputs of this chip, and output 1 will randomly work or not work. Each time the chip is powered up, or the output is switched on through ENSW1, there's a random chance that it will…
Hi Dimiti,
Thank you for your interest in WEBENCH. Currently WEBENCH has limited support for PMU devices. Also transient simulation is not enabled in WEBENCH for this device - we only have bode plot. I updated the panel in design and development section…
Part Number: TPS65400-Q1 Other Parts Discussed in Thread: TPS65400 , TPS544B20 , TPS544B25 , LM3000 , TPS40192 Dear Sirs,
I have developed a module with one TPS65400 to provide 3 output rail for a FPGA board: +1V, +3.3V and 2.5V (buck 1 and buck 2 in shared…
Part Number: TPS65400 Tool/software: Hello,
My customer is testing the TPS65400 operation on a board they designed as shown in the circuit below.
TI_PMIC_TPS65400RGZT.pdf .
When they measured VDDA, VDDG, and VDDD after inputting VIN 12V and CE high according…
Part Number: TPS65400-Q1 Hi sir,
Our customer have a question about the TPS65400-Q1 part numbered product. it is indicated that the product is qualified for the : –40°C to 125°C ambient operating temperature on the first page of the datasheet.…